cancel
Showing results for 
Search instead for 
Did you mean: 

Compiling C for ST7

awaller24
Associate
Posted on March 05, 2007 at 04:46

Compiling C for ST7

2 REPLIES 2
awaller24
Associate
Posted on March 04, 2007 at 23:46

I've just been given a ST72F345C4 to program, using a FLASH STICK

programmer. I only want to write simple programs, so I tried to compile

my code with ''ST7 Visual Develop'', I have set up a project, wkspace,

etc and including header files.

BUT. I keep getting these linker errors:

#error clnk example.lkf:14 can't open file crtsx.st7

#error clnk example.lkf:15 can't open file libim.st7

#error clnk example.lkf:16 can't open file libm.st7

*** Is it a problem with the linker or is there a greater problem with

only using this program? Must I use Cosmic/ Codewarrior/ something else

to compile? ***

I did a search in the root ST7 directory and none of these files are

even there! I also tried to download Cosmic Compiler for ST7, but there

link is broken. any suggestions??

Thanks. :-o

luca239955_st
Associate III
Posted on March 05, 2007 at 04:46

Quote:

#error clnk example.lkf:14 can't open file crtsx.st7

#error clnk example.lkf:15 can't open file libim.st7

#error clnk example.lkf:16 can't open file libm.st7

these are files that belong to the Cosmic compiler installation, so, yes, you need to install the Cosmic compiler

Quote:

I also tried to download Cosmic Compiler for ST7, but there

link is broken.

Our website had a problem in the second half of last week, it should be back to work today. Sorry for the inconvenience.

Regards,

Luca (Cosmic)