2006-10-11 07:58 PM
accessing external memory,hitex emulator
2006-10-09 09:24 PM
Hello Friends,
Debugging code for st10f276 using hitex emulator(dprobe167. While downloading to the emulator, getting error ''cannot acces external memory''. So i cudn't able to download. ofcourse, I downloaded the code for standalone image. So what are changes i have to do in registers in to download it to external memory (hitex xpermodule memory). Looking thro , one the discussion , one of you used hitex emulator if possible can you give me what are the register and values to be set in startupcode. Thanks, vijay. ESDS pvt limited2006-10-10 01:06 AM
Hello Neila,
Plz kindly look into the test system info. I have also sent mail to you. I set the value of syscon register thro script file. It would be nice if i have some sort of demo. I'll be waiting for your reply. Thanks & regards, vijay On 10-10-2006 at 12:01, Anonymous wrote: Hello ESDS, Could you please give me more information regarding the following points: - Which address space is used for the emulation memory? - What is the setting used for the DProbe? Could you give the Hitop System Info. (SYSTEM -> TEST SYTEM INFO)? Regards, Neila ________________ Attachments : testinfo.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0At&d=%2Fa%2F0X0000000bYq%2F51nVj1om3KzjPXNy1I.LCVuJJoitQ4KtRl0HstpjQes&asPdf=false2006-10-10 01:37 AM
Hello Neila,
Plz kindly look into the test system info. I have also sent mail to you. I set the value of syscon register thro script file. It would be nice if i have some sort of demo. I'll be waiting for your reply. Thanks & regards, vijay2006-10-11 07:58 PM
Hai,
Atlast , i have done it. It is because of Xram bit not enabled in the xperemu register. I am really ashamed for this. Next time i should check this first. Thanks vijay