missing-QuestionPost

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

looking for engineer

We are a dental manufacture . We are located outside Philly. We need engineering help. We will design a brush less , sensor less controller using the st32 chip.

alieb by Associate
  • 371 Views
  • 0 replies
  • 0 kudos

I'm using S2-LP with Bluenrg2 and when I send out a message, it only sends one frame whereas it is supposed to send 3 frames of the same message and sequence number.

I'm using SIGFOX_API_send_frame((uint8_t *)(&Data_Pkg),12,customer_resp,0,0);to send the message. According to Sigfox, Each Sigfox message will always be sent in 3 repetition (each repetition is considered a frame) with the same message content on di...

CChon.0 by Associate II
  • 364 Views
  • 0 replies
  • 0 kudos

Resolved! Where to find Radio driver for spbtle-rf0

I want to build a BLE repeater using the ​spbtle-rf0 module, I am using the x-nucleo-idb05a1 expansion board for the development. I saw that a radio driver is available for bluenrg-1 and bluenrg-2 modules but couldn't find it for spbtle-rf0 which is ...

How to program STUSB4700 on a custom board?

Does the IC have to be powered through VDD or can it be powered through V_SYS? I tried powering the IC through V_SYS and connecting the I2C pins to Nucleo-F072RB and en.stsw-stusb001 GUI. My custom board is not detected (attached schematic for your r...

ABysa by Associate II
  • 1686 Views
  • 5 replies
  • 0 kudos

Disabling of "Generation application code"

Hi,I would like to say if it is possible to disable the automatic generation of the application code because it always overwrites what I change. For example, if I change something inside a driver file, when I compile, at first it automatically overwr...

MMont.15 by Associate II
  • 425 Views
  • 1 replies
  • 0 kudos

SPBTLE-1 range & discoverability issue.

@Piotr Romaniuk​ @Winfred LU​ I have been using SPBTLE-1s module for a month or so. I have been experiencing failure in discovering the module whilst scanning and whenever i move closer to the module the it shows up. I have setup the TX level to 8 dB...