2019-03-19 8:32 PM
@Piotr Romaniuk @Winfred LU
I have been using SPBTLE-1s module for a month or so. I have been experiencing failure in discovering the module whilst scanning and whenever i move closer to the module the it shows up. I have setup the TX level to 8 dB but the situation has not improved. I know the indoor distance supported by BLE v4.2 is 10 m but my testing distance is almost 4-5 m . Also the outdoor connection is maintained for 4-5 m only.
Thanks
Altamash
2019-05-01 8:57 PM
Hi Altamash,
Could you please follow the HW design suggestions in datasheet:
The area around the module should be free of any ground planes, power planes, trace routings, or metal for 6 mm from the module antenna position, in all
directions.
Please also have local FAE help review your design.
Thank you.
Best Regards,
Winfred
2019-05-01 10:41 PM
Hello Winfred,
We have already incorporated the above mentioned suggestions in our designs, although we not got it reviewed from the local FAE.
Thanks for the suggestion. Feel free to provide any more suggestions.
Thanks
Altamash Abdul Rahim