2019-10-28 6:17 AM
Hello,
When I am trying to login to Unicleo GUI I am able connect to the communication port but the firmware description, version, expansion board name and library version in the login screen is showing unknown and I am not being able to connect expansion board( I am using stm nucleo F401RE and the Nucleo –IKS01A2 expansion board).In the user messages it is showing that the successive port is being opened but I am not been able to get any communication with the expansion board as such .Kindly note that I have already downloaded the virtual port driver as well.
Can anyone please help me figure out the Unicleo with IKS01A2 expansion board working ?
2019-10-28 6:56 AM
Hello @Eleon BORLINI,
Can you please support me on this?
2019-10-28 9:31 AM
Hi @User_of_Sensor , are you sure your COM4 is not already occupied by other peripherals? Btw, I invite in the discussion @Miroslav BATEK , who is the maximum expert of the Unicleo-GUI. Regards
2019-10-30 1:33 AM
You have to first program the Nucleo board with firmware from X-CUBE-MEMS1 package. In this package you can find DatalogExtended firmware which you can use for sensor testing and many applications which can be used for motion libraries evaluation.