cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO or LSM6DSOX?

ontares
Associate

Hi everyone,

is possible to determinate which module is mounted between LSM6DSO or LSM6DSOX reading some registers?

Thanks and Best Regards,

Leonardo M.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @ontares​ , there is a reserved register, the 1Fh, in the DSOX which is an identifier. while the same register is used as slave3 address in the DSO. So should be equal to 00h in DSO. Btw the easiest way to see the difference is to read the top package marking:

  • S0 for DSO
  • S4 for DSOX

In general, please note that the main difference between the two pn is that the Machine learning core (MLC) embedded feature is working on DSOX while is not working on DSO. Regards