2020-04-20 4:10 AM
Hi!
I found a thread that says thtat the ST-LINK/V2 can be used as in circuit programmer.
SensorTile.box firmware OTA function restore documentation says that the programmer, a JTAG adapter board V1.0 and a Flat cable to connect JTAG adapter to SensorTile.box is needed.
The SensorTile.box user manual says in chaper 3.3: "... and the most recent release of the Sensortile.box includes an adapter board and cable for the ST-LINK/V2 programming and debugging device."
I ordered two devices of the SensorTile.box but there was no adapter or cable included. Can you give me information where to get those? I could not find them anywhere as separate parts. Are they part of the STLink/V2 package?
And another question: There is a UART for debugging purposes on SensorTile.box pins available. Can I use the STLink/V2 directly to read from those pins with my PC and a serial console? Or do I need a separate converter?
Best wishes,
Dominik
Solved! Go to Solution.
2021-04-16 1:17 AM
Hi @KBada.1 ,
that's strange... did you purchase it on the ST eStore?
If so, let's try to manage a shipment to your address. You can write it to me in the Message section (the menu at top right of the page, under the profile picture).
-Eleon
2020-04-20 6:49 AM
Hi @DWind.1 , when did you ordered the two SensorTile.box packs? If you did in the last period, you should have received something like the kit depicted here below:
Regards
2020-04-20 7:34 AM
Hi! I ordered 08.01.2020 at Mouser. I received a package like in this video: https://www.rs-online.com/designspark/unboxing-the-sensortile-box-from-stmicroelectronics-1 without adapter and cable.
2020-04-21 8:46 AM
Hi Dominik, maybe the Mouser stock was not provided by the newest SensorTile.box kits, in that date.
Can you please share me your address? We can ship you one adapter + one cable (at least when the lockdown is over).
Regarding your other question:
>> There is a UART for debugging purposes on SensorTile.box pins available. Can I use the STLink/V2 directly to read from those pins with my PC and a serial console? Or do I need a separate converter?
Please note that the STLINK-V2 is not capable of UART communication for the debugging, but you need the STLINK-V3 programmer. However, STLINK-V3 is 3V compatible, while SensorTile.box is 1.8V compatible. This adapter with the digital level shifters will be soon available online.
Regards
2020-07-02 6:37 AM
Hello Eleon,
we've ordered 4 pieces in May at Mouser, also got the old ones without adapter and cable
BR
2020-07-02 6:54 AM
Uhm strange... let me check internally...
@DWind.1 , sorry for the delay, we have had an issue in our stores related to the shipment of the STWIN adapter. Should manage the shipment by next days...
Regards
2020-07-02 6:55 AM
The same here, I ordered one @ mouser last week and received this. I need to upload the software, the unit lost control during an over-air code update.
2020-07-14 1:16 PM
Same as well. No adapter, no cable. Shipped from Mouser 2wks back
2020-07-16 5:29 AM
Hi @KPauw.1, @avoyt.1 , I'll ship you a cable if you share me your shipment address. You can use the private message section. Regards
2020-07-16 8:06 AM
***Edited by moderation to remove contact details***