2024-10-28 09:50 AM
Hi All,
My name is Stefano, and I developed firmware for an embedded sensor that integrates the LIS2DW12 MEMS accelerometer. We encountered the following issue:
Main resin infos are follows:
shore A hardenss of 74-80,
Dielectric Costant 7-8,
Dielectric Strength of 22 to 23 kV/mm,
water absorption rate of 0.2%-0.3% after 24h at 25°C
Main resin infos:
Name MOMENTIVE TSE397 seires
Shore A hardness of 20
Dielectric Costant 2.9
Dielectric Strength of 22 to 23 kV/mm
Can you tell us what we can do in order to resinate our sensor and avoid axtra current absorption?
P.S. attached you can see one of the conformal coated sensors.
Thanks in advance.
2024-11-08 06:00 AM
Hi @Stefano_82 ,
300mA is a very high value that we do not expect can be handled by the device. By retesting do you always get this value?
2024-11-11 08:56 AM
Hi Federica,
Thanks for answering my question. As I mentioned in my first post, I have a lot of sensors with very strange behaviors in my office.
Normally, our sensors work at 7-10mA, but the faulty sensors (only with the integrated accelerometer) have different absorption behaviors.
Most of them work at 80mA, and if I touch the resin, the current absorption rises to 200mA and slowly fall down to 80 mA. Some have an absorption of 200mA, and others at 300mA.
Unfortunately, I'm currently out of the office for work and can't provide you with the log of the sensors with 300mA of absorption. However, I can give you a log of one of them that I stored locally.
This is the current absorption with the sensor fully resinated and the accelerometer powered up in sleep state:
Normally, its current absorption is under 10mA, and if I power off the accelerometer its absorption returns to normal ranges.
Do You have te possibility to open the .ppk2 extension files?
Is there a possibility to have a private ticket discussion?
Thanks in advance.
2025-01-10 11:09 AM
Hi Stefano,
Do you still have this issue? We have a similar one LSM6dsm instability and high current consumption. You can try our solution (adding 300pF capacitors), or, if you have pull-pus or pull-downs, to replace them with direct driving by push-pulls in the software. Do you have a schematic that you can share by any chance?