2024-03-17 11:51 PM
Hi
I'm currently using your LPS22DFmodule to measure pressure and I saw in the datasheet that the temperature accuracy is ±1.5 °C (T = 0 to 80°C). My working range is between -15°C and 60°C. Could you please give me the accuracy of this sensor in the range -15 to 65°C?
Solved! Go to Solution.
2024-04-04 06:17 AM
Hi @ljm ,
We tested few parts and I confirm you that the accuracy was around 2°C but consider that we considered a limited number of pcs and thus this value can't be guaranteed in production.
2024-03-18 12:51 AM
Hi,
pressure - from ds:
2024-03-18 01:24 AM
hello @AScha.3
thanks for replying.
I'm speaking about the temperature accuracy.. in the datasheet it is ±1.5 °C (T = 0 to 80°C), but my working range is betwwen -15°C and +60°C... just if it's possible i want to know the accuracy is the same between -15°C and 0°C or h
greater than the accuracy betwwen 0°C and 80°C ?
Thank you in advance
2024-03-18 01:54 AM - edited 2024-03-18 02:00 AM
>if it's possible i want to know the accuracy
Its not specified, so test it yourself, to know for sure.
Anyway at +/-1,5° this is more guessing "temp. is about" , so if you want measure temperature, take a temperature sensor to do this (and not a pressure sensor).
I use the ENS210 , temp. + humidity :
Or a pressure + temperature sensor, like BMP280 (or BME280 etc. ); this can with some interpolation give a temperature resolution of 1/1000 ° ! (I tried, is funny, you can see when your go to the table, the bmp280 is there, temperature rising about 0,003° - from body IR radiation ! )
2024-03-19 02:03 AM
Hi @AScha.3
Thanks for replyin.
in my application i want to mesure pressure and temperature , the ENS210 is a humidity /temperature sensor.
By the way the BMP280 is not avaible
2024-03-19 02:41 AM - edited 2024-03-19 02:48 AM
Hi,
ENS210 - just example, for $2 temp (+hum.) sensor;
+
BME280 - i wrote also - more new + expensive....but: mouser has 12000...
BME280 Bosch Sensortec | Mouser Deutschland
(Its typical used in cars, sensing air conditions for perfect fuel injection control.)
+
For any cheap+good temp.sensor - there are many:
Temperatursensoren für Plattenmontage – Mouser Deutschland
+
If +/- 3° are ok for your app - take the LPSS22DF ; just test at lowest temp, to be sure.
(Anyway it should be better, because datasheet gives minimum value .)
2024-03-19 07:47 AM
Hi @AScha.3
thanks for replying,
actually i'm using LPS22DF , just i want to know it temperature accuracy for negative values because on datasheet the temperature accuracy is +-1.5 °C from 0°C to 80°C , but the range of my application is -15°C to 60°C , just i want to know what the temperature accuracy for negative values
2024-03-26 06:33 AM
Hi @ljm ,
You don't find this data because on the range -20 to 0 °C it is tested only in characterization and thus not guaranteed in production.
2024-03-26 06:58 AM
thanks for replying
does this mean that lpss2df is not accurate between -20°C and 0°C? is it not advisable to use it in this range?
thanks
2024-03-26 07:06 AM
No, LPS22DF can be used in the range -40 to +85 °C and it is also accurate.
However, we do not provide a typical reference value because in that range the sensor was only tested on a limited number of pieces and therefore we could not guarantee the same value on a large number of samples as in production.