2022-09-09 05:36 PM
This video is really good, and details how to integrate the IKS01A3 with the NUCLEO-WL55JC.
Beyond this, there is no documentation re what other expansion boards can integrate with the NUCLEO-WL55JC.
In fact other expansion boards explicitly indicate the specific boards they do integrate with. And none of them indicate NUCLEO-WL55JC.
To make the NUCLEO-WL55JC useful, it will require expansion boards. Is this info somewhere? Is there a roadmap?
2022-09-09 05:49 PM
Perhaps there are schematics and pin-lists, and you could connect the dots?
2022-09-09 07:45 PM
I wouldn't really have a problem with tracing the hardware, as you suggest.
It's the software. There is no info on any software support for any other expansion board on the NUCLEO-WL55JC board.
Maybe the intention is to push the market toward the I-NUCLEO-LRWAN1, which is supported on a few boards, and does look like a better overall approach. It's just not available to buy right now (1 year b/o on mouser).
2024-01-03 06:50 AM - edited 2024-01-03 07:14 AM
W