cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DE12

NItin Kanani
Associate II
Posted on January 04, 2018 at 08:44

I am interfacing sensor with Micro controller and controller is working at +3.3V.

VDD_IO and VDD are two power supply pins in sensor.

If i am giving common supply +3.3V of controller to VDD_IO and VDD , will it work?

OR

Do i need to give seperate voltages for both supply pins?

Suggest me.

Thanks.

1 REPLY 1
Miroslav BATEK
ST Employee
Posted on January 04, 2018 at 09:19

Yes, it will work. You can tie VDD_IO and VDD together and connect both to 3.3V.