2021-12-17 3:12 AM
2021-12-17 3:21 AM
Yes, you can feed data from the internal ADC into DFSDM and process it there, see Digital filter for Sigma-Delta Modulators (DFSDM).
Regards
/Peter
2021-12-17 3:21 AM
Yes, you can feed data from the internal ADC into DFSDM and process it there, see Digital filter for Sigma-Delta Modulators (DFSDM).
Regards
/Peter
2021-12-20 3:30 AM
@Peter BENSCH Thanks for sharing the information. IS there is any document or application note to set DFSDM parameters in MX Cube like Filter 0 or Filter 1 , DMA setting and Channel Selection and the mode like -> pareller or manchester so on
2021-12-20 5:00 AM
You will find loads of information also in RM0432, e.g. section 21.4.27 and especially section 28.
Unfortunately, ST cannot offer a tutorial at the moment, but the reference manual is actually a perfect textbook for this.
Regard
/Peter
2022-01-11 10:07 AM
By the way: have you seen the training material STM32L4+ Online Training that could also be helpful as a supplement to the reference manual?
Just search for DFSDM and either listen to the presentation (blue triangle) or read the PDF (red icon to the right).
Regards
/Peter