2021-11-18 6:54 AM
2021-11-23 2:57 AM
Hi, probably there is no predefined example with the NUCLEO-F303RE + IKS01A3, even if the two boards are compatible.
You might start from the FP-SNS-ALLMEMS1, where there is an example with an evaluation board with STM32 Cortex M4 (STM32F401RE-Nucleo). From this example, you can configure the peripherals for the interface with the IKS01A3 expansion. The Arduino R3 connector is the same across all Nucleo boards.
2021-11-23 2:57 AM
Hi, probably there is no predefined example with the NUCLEO-F303RE + IKS01A3, even if the two boards are compatible.
You might start from the FP-SNS-ALLMEMS1, where there is an example with an evaluation board with STM32 Cortex M4 (STM32F401RE-Nucleo). From this example, you can configure the peripherals for the interface with the IKS01A3 expansion. The Arduino R3 connector is the same across all Nucleo boards.
2021-11-25 8:57 AM
Hi @AWall.4 ,
welcome to ST community then!
Did @TSand.1 answered your question? I would have answered pretty the same things.
-Eleon