Skip to main content
HY.1
Visitor II
March 24, 2022
Question

What value is the beam waist(radius) of the VL53L5CX TX light? As we are going to do further development based on VL53L5CX ,could you please share more information about the TX light beam?Just like the M2,the beam waist and so on.

  • March 24, 2022
  • 1 reply
  • 638 views

..

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
March 25, 2022

That is quite a question. The light from the laser goes out in a 27 degree cone. But a diffractive optical element spreads the light to what we say is a 45 degree pyramid. A wall at 1M will have a square of illumination 1M on a side. But that 45 degrees is the edge of full power. It's where the roll-off starts to happen, At 60 degrees there is really not much detectable light, but to insure there is no light, you have to go most of the way to 90 degrees off center. Generally this roll off doesn't matter. But if you were to place a reflective object within the rolloff area you could get some crosstalk issues depending on the optical nature of that object.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.