cancel
Showing results for 
Search instead for 
Did you mean: 

Are the algorithms provided by ST, such as MotionFX, open source or closed source? Is the user able to develop their own algorithms?

ILARIASOFIA.GRASSI
ST Employee
1 ACCEPTED SOLUTION

Accepted Solutions
Denise SANFILIPPO
ST Employee

The Motion libraries are not open source and are provided in binary format. However, ST provides also open-source examples such as IIR filter and CRC computation. The user is free to develop their own algorithms: the ISPU can be programmed in C code to implement any type of processing.

View solution in original post

1 REPLY 1
Denise SANFILIPPO
ST Employee

The Motion libraries are not open source and are provided in binary format. However, ST provides also open-source examples such as IIR filter and CRC computation. The user is free to develop their own algorithms: the ISPU can be programmed in C code to implement any type of processing.