2023-05-19 05:35 AM
Q&A - webinar "In-sensor monitoring with intelligent MEMS sensors"
Solved! Go to Solution.
2023-05-19 05:53 AM
The Motion libraries are not open source and are provided in binary format. However, ST provides also open-source examples such as IIR filter and CRC computation. The user is free to develop their own algorithms: the ISPU can be programmed in C code to implement any type of processing.
2023-05-19 05:53 AM
The Motion libraries are not open source and are provided in binary format. However, ST provides also open-source examples such as IIR filter and CRC computation. The user is free to develop their own algorithms: the ISPU can be programmed in C code to implement any type of processing.