cancel
Showing results for 
Search instead for 
Did you mean: 

Configuration TuochGFX STM32F469I-DISCO for STM32Cube IDE

DEspo
Associate

Hello,

 we are working with a STM32F469I-DISCO board and the new STM32CubeIDE.

We have followed some discussion in the community (mainly for the STM32F746).

The board seems configured correctly, after the command:

otm8009a.c

/* Send Command Display On */

DSI_IO_WriteCmd(0, (uint8_t *)ShortRegData44);

otm8009a.h

const uint8_t ShortRegData44[] = {OTM8009A_CMD_DISPON, 0x00};

the display shows the following image:

But then we couldn't see our UI, it seems that the OS is stopped after the entryEvent of the GUI:

void TGFX_GuiTask(void * argument)

{

   touchgfx::HAL::getInstance()->taskEntry();

}

1 REPLY 1
SBERT
Associate II

Hello,

I have exactly the same problem.

Keep me updated please :)

Thanks

Sam