cancel
Showing results for 
Search instead for 
Did you mean: 

Could you provide the VL53L0X/L1X Laser Safety IEC 60825-1:2014 Compliance Report?

MFabb.1
Associate II

Our products integrate the above PNs and we would need these documents in order to submit them to the cerification laboratory.

As reported in the datasheet both ToF sensors are "designed to remain within Class 1 laser safety limits under all reasonably foreseeable conditions including single faults in compliance with IEC 60825-1: 2014 (third edition)."

0693W00000D152uQAB.png 

0693W00000D14xMQAR.png 

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

here you go...

This is the report we filed with the FDA certifying class 1.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

3 REPLIES 3
John E KVAM
ST Employee

here you go...

This is the report we filed with the FDA certifying class 1.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
MFabb.1
Associate II

Thank you John.

JB..1
Associate

Hi John,

I had a look at the attached report but Attachment 2 seems to be removed from the document. Is there any possibility to get it? There are references to this attachment in the test report (Part 8) and contains information that would be useful for us.

Thank you,

Jimmy