2021-07-30 1:53 AM
Our products integrate the above PNs and we would need these documents in order to submit them to the cerification laboratory.
As reported in the datasheet both ToF sensors are "designed to remain within Class 1 laser safety limits under all reasonably foreseeable conditions including single faults in compliance with IEC 60825-1: 2014 (third edition)."
Thank you
Solved! Go to Solution.
2021-08-09 4:51 PM
here you go...
This is the report we filed with the FDA certifying class 1.
2021-08-09 4:51 PM
here you go...
This is the report we filed with the FDA certifying class 1.
2021-08-29 11:52 PM
Thank you John.
2022-08-25 6:21 AM
Hi John,
I had a look at the attached report but Attachment 2 seems to be removed from the document. Is there any possibility to get it? There are references to this attachment in the test report (Part 8) and contains information that would be useful for us.
Thank you,
Jimmy