cancel
Showing results for 
Search instead for 
Did you mean: 

What is the easiest way to measure distance by using VL53L3CX?

Idede.1
Associate

I have tried to use drivers and example code which are provided by STM in website. My board is P-NUCLEOWB55, and example codes are written for STM32F401RE-Nucleo and STM32L476RG-Nucleo. When I call the HAL_I2C_IsDeviceReady() function, it returns HAL_OK. And also all driver functions which I used in below code these returns zero. But I could not get any measurement result.

What is the most simple way to measure the distance by using this sensor?

What is the suitable way to integrate sensor driver to the project? (When I compile it, it does not give any error but maybe I made mistake when I put driver files to the project.)

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * <h2><center>&copy; Copyright (c) 2021 STMicroelectronics.
  * All rights reserved.</center></h2>
  *
  * This software component is licensed by ST under BSD 3-Clause license,
  * the "License"; You may not use this file except in compliance with the
  * License. You may obtain a copy of the License at:
  *                        opensource.org/licenses/BSD-3-Clause
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "vl53lx_api.h"
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
VL53LX_Dev_t dev;
VL53LX_DEV Dev = &dev;
int status;
volatile int IntCount;
 
I2C_HandleTypeDef hi2c1;
 
UART_HandleTypeDef huart1;
 
int16_t RangeMilliMeter;
 
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_NVIC_Init(void);
 
int main(void)
{
  uint8_t byteData;
  uint16_t wordData;
  uint8_t ToFSensor = 1; // 0=Left, 1=Center(default), 2=Right
 
  HAL_Init();
 
  Dev->I2cHandle = &hi2c1;
  Dev->I2cDevAddr = 0x52;
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  HAL_GPIO_WritePin(IR_RESET_GPIO_Port, IR_RESET_Pin, GPIO_PIN_RESET);
  HAL_Delay(10);
  HAL_GPIO_WritePin(IR_RESET_GPIO_Port, IR_RESET_Pin, GPIO_PIN_SET);
  HAL_Delay(10);
 
  VL53LX_MultiRangingData_t MultiRangingData;
  VL53LX_MultiRangingData_t *pMultiRangingData = &MultiRangingData;
 
  MX_GPIO_Init();
  MX_I2C1_Init();
  HAL_Delay(100);
  MX_USART1_UART_Init();
  HAL_Delay(100);
  MX_NVIC_Init();
  if(HAL_I2C_IsDeviceReady(&hi2c1, 0x52, 1, 10) == HAL_OK){ 
  	  HAL_GPIO_WritePin(GPIOB, LD1_Pin, GPIO_PIN_SET); // Blue LED
  }
  status = VL53LX_WaitDeviceBooted(Dev);
  HAL_Delay(2);
  status = VL53LX_DataInit(Dev);
  HAL_Delay(2);
  status = VL53LX_StartMeasurement(Dev);
  HAL_Delay(2);
 
  while (1)
  {
		  status = VL53LX_WaitMeasurementDataReady(Dev);
		  status = VL53LX_GetMultiRangingData(Dev, pMultiRangingData);
		  RangeMilliMeter = pMultiRangingData->RangeData[0].RangeMilliMeter;
 
		  if (status==0){
			status = VL53LX_ClearInterruptAndStartMeasurement(Dev);
		  }
 
  }
 
}
 
/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 
  /** Configure the main internal regulator output voltage
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
                              |RCC_OSCILLATORTYPE_MSI;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.MSIState = RCC_MSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_10;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
                              |RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the peripherals clocks
  */
  PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS|RCC_PERIPHCLK_USART1
                              |RCC_PERIPHCLK_I2C1;
  PeriphClkInitStruct.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
  PeriphClkInitStruct.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1;
  PeriphClkInitStruct.SmpsClockSelection = RCC_SMPSCLKSOURCE_HSI;
  PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLKDIV_RANGE0;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
}
 
static void MX_NVIC_Init(void)
{
  /* EXTI1_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(EXTI1_IRQn, 1, 0);
  HAL_NVIC_EnableIRQ(EXTI1_IRQn);
}
 
/**
  * @brief I2C1 Initialization Function
  * @param None
  * @retval None
  */
static void MX_I2C1_Init(void)
{
 
  hi2c1.Instance = I2C1;
  hi2c1.Init.Timing = 0x00707CBB;
  hi2c1.Init.OwnAddress1 = 0;
  hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
  hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
  hi2c1.Init.OwnAddress2 = 0;
  hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
  hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
  hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
  if (HAL_I2C_Init(&hi2c1) != HAL_OK)
  {
    Error_Handler();
  }
  /** Configure Analogue filter
  */
  if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
  {
    Error_Handler();
  }
  /** Configure Digital filter
  */
  if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
  {
    Error_Handler();
  }
}
 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Batuhan A.
Associate II

I'm also working on that issue. Is there anybody who knows the simplest way to read distance data? The driver is too much complicated.