Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X Measurement noise reduction?

I have two 3-element arrays on my 4-wheel robot, one on each side. I use the arrays for simple distance measurements, and also to orient the robot parallel to a nearby wall by turning it until the front and back VL53L0X sensors (separated by 8.5cm) ...

0693W00000WIanwQAD.jpg
FPayn.1 by Associate III
  • 3345 Views
  • 3 replies
  • 0 kudos

Resolved! VL6180X -- How to achieve a 100 Hz sample rate?

I have a VL6180X that I am running in continuous measurement mode and read from when a hardware interrupt is triggered by the senor. My issue is that I cannot get the sensor to signal at a rate of 100 Hz. Currently, the best I can achieve is 50 Hz.Ha...

Kurt-123 by Associate II
  • 3866 Views
  • 3 replies
  • 0 kudos

Help with insight on VL53L4CD drift

I'm using the VL53LX API 1.2.8 to interface with the VL53L4CD in firmware and I implemented a tuner page in my android app to visualize it.So far I have this thing ranging pretty well with +/- 1mm accuracy. Not bad!I'm measuring a permanent grey 3D p...

0693W00000WI44BQAT.png
AGreen by Associate II
  • 1887 Views
  • 2 replies
  • 1 kudos

about connection of pins in VL53L1X

Dear Sir,We are going to make our own PCB after confirming the action with X-NUCLEO-53L1A1 module. We found the connection of pins 4, 6 12 in VL53L1X breakout board is different with the Figure3 (VL53L1Xschematic) . In Figure 3, pins 4, 6 and 12 ar...

DSai.1 by Associate III
  • 1228 Views
  • 1 replies
  • 0 kudos

Strange behavior of the VL53L0CXV0DH sensor.

Strange behavior of the VL53L0CXV0DH sensor.I get the correct data (distance to the obstacle), with a normal change in the position of the obstacle (zoom in / out), the data changes correctly and corresponds to the real distance.If the obstacle is sh...

0693W00000Lwh1bQAB.png 0693W00000Lwh1WQAR.png
RPavl.2 by Associate II
  • 7473 Views
  • 18 replies
  • 0 kudos