Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there any way to know the basic control related commands of the VL53L5CXV0GC chip? Can't the st microelectronics customer technical support center help with this? If neither is possible, should I apply and use only the provided f/w for Eva Board?

I We purchased this sensor to apply it to our own board. I want to know the command to control the sensor on the board, but the data sheet only provides for simple i2c communication and address, index, and data structure.

YJu H.1 by Associate
  • 1379 Views
  • 2 replies
  • 0 kudos

Resolved! Help on issues found in VL53LX API v1.2.8?

I'm using the latest API version (1.2.8) available from the VL53L4CX product page.In my project I have implemented an interface to set configurations or run calibrations.I am also using this driver for both the VL53L4CD and VL53L4CX, since the driver...

AGreen by Associate II
  • 1847 Views
  • 2 replies
  • 1 kudos

Resolved! STSW-IMG035 Minimum Resource Requirements (DMIPS) on HOST MCU

Hi all,i'd like to know the typical resource requirements (mainly required computing power / DMIPS value) of running the TouchLessControl library (STSW-035) library on a host MCU. The GestureEVK-UM.pf mentions a typical RAM and FLASH footprint :I k...

0693W00000Sw5bFQAR.png
LK by Associate II
  • 1930 Views
  • 1 replies
  • 0 kudos

Resolved! Gesture recognition on VL53L5CX?

I have read that ST will be releasing code to show how to do gesture recognition on the VL53L5CX, when is this due to be released?

yzer.1 by Associate II
  • 2819 Views
  • 3 replies
  • 0 kudos

VL53L5CX: minimum size of an empty zone between 2 objects

Hi, I'd like to know what is the minimum size or gap between 2 objects the sensor is able to detect ? My first test shows a surface of 600 cm² seems to be the minimum, i.e a "hole" square of 25 cm x 25 cm or a rectangle of 20 x 30 cm.When I do the ma...

EPARM.1 by Associate
  • 1010 Views
  • 1 replies
  • 0 kudos

Gesture recognition with VL53L5CX

Good day, Is there currently any support for gesture recognition with the VL53L5CX ToF sensors, as shown in the Video "Gesture Tracking on Thermostat with VL53L5CX"?I could not manage to find any examples or information about how to implement this.Re...

DMeie.2 by Senior II
  • 2611 Views
  • 8 replies
  • 0 kudos