Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L7CX sensor - GO2 error status

Hello,We have an issue with the VL53L7CX. We are using 2.8V for both IOVDD and AVDD. We have 4x TOF sensor on the same I2C line. We set the LPn for 3x of them to low to disable the i2c comm. We are only using 1x TOF for now with it's LPn set to High ...

FB__1 by Associate III
  • 648 Views
  • 3 replies
  • 0 kudos

VL53L1X Interrupt not working, No measurements

Hi, I am having trouble with the interrupt. I manange to coummunicate via I2C and read Model ID and Type. But my problem is that i can't initiate the sensor via the VL53L1X_SensorInit() function in the Ultra Lite Driver I'm using. When I debug I see ...

Resolved! Strange start-up behaviour of VL53L5CX ToF sensor

Hello Developers, Hello ST-Team,unfortunately we are stuck in implementing VL53L5CX on our PIC18. We see a strange clock stretching behaviour of the sensor and problem downloading the firmware.We implemented Ultra Lite Driver 2.0.0 in an application ...

Joh70_0-1746790956757.png Joh70_1-1746791711071.png Joh70_0-1746793224931.png Joh70_2-1746791875643.png
Joh70 by Associate II
  • 2066 Views
  • 5 replies
  • 0 kudos

vd55g1 - no data in stream mode

Hi, I'm currently facing a challenge with the VD55G1 driver. I've designed my own minimal system board for the N6 and VD55G1, using MIPI CSI for communication. When attempting to drive the VD55G1, I can enter the stream mode but no data is being tran...

eureka_0-1753080705782.png eureka_1-1753080722856.png eureka_2-1753080734553.png
eureka by Associate II
  • 1267 Views
  • 5 replies
  • 0 kudos

STSW-IMG501 Booting From Script Fails

I am using the STSW-IMG501 software v1.1.1 with the STEVAL-EVK-U0I connected to a STEVAL-56G3MAI (the S-board evaluation module for the VD56G3).  In the EVK software, I am using the built-in script generation tool to upload different register configu...