Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L4CX Additional Infos

Hello everyone out there,I hope one of you can help me because I'm a bit confused about the additional information the sensor provides.I need to measure the fill level of a salt container. I noticed that the measured values deviate by about 6 cm comp...

Resolved! VL53L4CD Power consumption measurement

Hello Everyone, I'm using the VL53L4CD with the STM32WL55JC1, The following is the Power Profile of the cycle:1- XSHUT GPIO is normally pulled low.2- XSHUT Pulled up + delay ( sensor wakes up).3- VL53L4CD Initiliazation.4- Measurements (20 Samples).5...

AElgh_0-1701856490333.png
AElgh by Associate III
  • 3834 Views
  • 6 replies
  • 1 kudos

VD6281 overexposure read value

Hi All,I am trying to implement VD6281 readout layer and I do struggle with quite random '0' return value with relatively intense light exposure.The implemented script automatically adjust sensor gain. For relatively high register values [15..12] wha...

Mks1 by Associate II
  • 777 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1CB - ROI (Region of Interest) must be configured ?

VL53L1CB必须配置其 ROI(感兴趣区域)以定义要读取的“单元格”网格。如果不设置 ROI,则只能获得一个合并的距离值,该值将来自所有 SPAD 的信号求和,并且您将无法获取每个子区域的解析数据。上述说法正确吗?Please note that the official forum language it English - see the Community Terms & Conditions.Google Translate:The VL53L1CB must have its RO...

labubu by Associate II
  • 684 Views
  • 4 replies
  • 4 kudos

Resolved! VL53L1X ULD API license question

We plan to implement a VL53L1X driver based on this API for our Open Source Real-Time OS (community project) and would have to publish the API source code (content of directory STSW-IMG009_v3.5.4/API only) either as part of the GitHub repository of t...

Running two Adafruit VL53L4CD with Arduino R4 WiFi

I've been trying to get two Adafruit VL53L4CD's to work without a multiplexer on my Arduino R4 WiFi, and am getting stuck after getting one reading. I'm largely drawing on the code discussed here, and have also changed up the bits that nh1628 discuss...

Untitled-drawing
eclemmon by Associate II
  • 1349 Views
  • 4 replies
  • 0 kudos

Resolved! Using CNH for Advanced Detection with VL53L8CH

Hi there, we recently purchased the VL53L8CH and are hoping to take advantage of its advanced capabilities for use in a small embedded product (without having to use a desktop GUI or large ST expansion board).Can you tell us more about the advanced A...

VL53L7CX Range Sigma Factor

Hi, I am currently testing the VL53L7CX ToF sensor. During my evaluation, I came across the parameter "range sigma", but I could not fully understand what it actually represents.In addition, while creating a correlation map, I noticed that the most i...

Cafko by Associate
  • 1057 Views
  • 3 replies
  • 0 kudos

VL53L5CX outdoor performance (or a suggested alternative)

I'm currently trying to use the VL53L5CX to detect motion in the range of about 1m in front of the sensor.This seems to work fine indoors - but outdoors - I don't seem to be able to get anything more than around 30cm, even with xtalk calibration, and...

zz9pa by Associate
  • 909 Views
  • 2 replies
  • 1 kudos