Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Register Map for VL53L8CX

I am trying to use VL53L8CX with stm32f4 discovery but had no success.  Implementing the preexisitting API has been tough.  Is there a register map for this sensor whcih can be used to create a minimalistic driver and interface sensor using I2C or SP...

Rituraj by Senior
  • 2757 Views
  • 5 replies
  • 2 kudos

Resolved! VL53L4cd not able to detect dark surface

I am trying to use VL53L4CD to detect whether there is a car on top of the sensor or not...I am placing my sensor on the ground and trying to detect if a car is parked on top of the sensor. But it is not able to detect the cars bottom surface. Howeve...

pthakkar by Associate II
  • 1451 Views
  • 6 replies
  • 2 kudos

Resolved! I'm confused about ST nomenclature for VL53L7CH

    I want to try the VL53L7CH, I purchased the SATEL-VL53L7 and the x-nucleo-53l7A1. When I look at the boards on the SATEL-VL53L7 they look identical. But the description says it supports both the CX and CH models. Can someone clear this up?

VD55G0 Video mode

According to the UM2829 manual stating that it supports "SLAVE_I2C STREAMING on I²C pulses", I would like to ask whether this means that image data can be obtained via I2C like the VD55G1, or if it only refers to synchronization signals between image...

eureka by Associate II
  • 957 Views
  • 4 replies
  • 0 kudos

Resolved! VD56G3 optical flow

Hi we are looking for optical flow sensor and try to configure VD56G3 camera for this purpose which is connected to rasberry pi 4.I came across research artice which states that it does support optical flow using  MIPI CSI-2 interface.https://arxiv.o...

ketchyn_0-1731960372161.png
ketchyn by Associate
  • 2214 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L7CX gesture detection

Hi, I am trying to use the VL53L7CX to do gesture detection for a household product. A few questions:Do these software downloads only run on a Windows PC? https://www.st.com/en/embedded-software/stsw-img035.html ? I am trying to do embedded developme...

Resolved! VL53L4CX Additional Infos

Hello everyone out there,I hope one of you can help me because I'm a bit confused about the additional information the sensor provides.I need to measure the fill level of a salt container. I noticed that the measured values deviate by about 6 cm comp...