2025-04-02 10:44 AM
Hello ST Team!
In one of my new projects i use the VL53L0X TOF Sensor to measure simple distances.
The mcu i use is the STM32F103.
To get values from the sensor i use the ST API Library. It's kind of s special version since i use the modified one which is working with the Cube MX Hal.
This is the repository i cloned and pointing to the master branch:
As this project is for the L4 i just replaced the hal include from
in the vl53l0x_platform.h file.
1. The INIT VL53L0X_PROXIMITY_Init() finishes without errors
2. The problem occurs when i do VL53L0X_PROXIMITY_GetDistance()
Within the function VL53L0X_calc_timeout_mclks() the division by zero fault occurs and i don't know exactly why since the range measurement is already done correctly.
Following depicts the callstack before the divsion happens.
Additionally the "DeviceSpecificParameters"
If I work around this the next division by zero is following immediatly.
Can you give me some hints why the zero division is happening?
Do i have to set some parameters as mentioned here? : VL53L0X Divide by Zero error in API - STMicroelectronics Community
Problem is that i do not have the VL53L0_i2c_platfform.c platform files.
Thank you in advance!
Regards, Lukas
2025-04-02 12:01 PM
I doubt yours is the same error. His was a porting error and you are using an STM32, so the timing functions should work.
I will grant you that one really should follow the advice in that issue though.
"...by checking for a zero value (and setting to 1) before doing the (divide)."
But yours is the first mention I've heard of in 4 years, so I'm going to guess it's your configuration.
Although I really can't point to where you might have gone wrong.
Could you post all your sensor initialization calls?
I'm betting there is something amiss in those.
- john
2025-04-02 12:34 PM
Thank you for your fast reply!
1. VL53L0X_PROXIMITY_Init();
2. VL53L0X_PROXIMITY_GetDistance();
This is the Init routine:
/**
* @brief VL53L0X proximity sensor Initialization.
*/
static void VL53L0X_PROXIMITY_Init(void)
{
uint16_t vl53l0x_id = 0;
VL53L0X_DeviceInfo_t VL53L0X_DeviceInfo;
/* Initialize IO interface */
//SENSOR_IO_Init(); --> I2C is already initialized in main.c
VL53L0X_PROXIMITY_MspInit();
memset(&VL53L0X_DeviceInfo, 0, sizeof(VL53L0X_DeviceInfo_t));
if (VL53L0X_ERROR_NONE == VL53L0X_GetDeviceInfo(&Vl53Instance, &VL53L0X_DeviceInfo))
{
if (VL53L0X_ERROR_NONE == VL53L0X_RdWord(&Vl53Instance, VL53L0X_REG_IDENTIFICATION_MODEL_ID, (uint16_t *) &vl53l0x_id))
{
if (vl53l0x_id == VL53L0X_ID)
{
if (VL53L0X_ERROR_NONE == VL53L0X_DataInit(&Vl53Instance))
{
Vl53Instance.Present = 1;
SetupSingleShot(Vl53Instance);
}
else
{
printf("VL53L0X Time of Flight Failed to send its ID!\n");
}
}
}
else
{
printf("VL53L0X Time of Flight Failed to Initialize!\n");
}
}
else
{
printf("VL53L0X Time of Flight Failed to get infos!\n");
}
}Additional Msp Init function and the GetDistance function
/**
* @brief VL53L0X proximity sensor Msp Initialization.
*/
static void VL53L0X_PROXIMITY_MspInit(void)
{
// done at hal init
//GPIO_InitTypeDef GPIO_InitStruct;
//
///*Configure GPIO pin : VL53L0X_XSHUT_Pin */
//GPIO_InitStruct.Pin = VL53L0X_XSHUT_Pin;
//GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
//GPIO_InitStruct.Pull = GPIO_PULLUP;
//GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
//HAL_GPIO_Init(VL53L0X_XSHUT_GPIO_Port, &GPIO_InitStruct);
HAL_GPIO_WritePin(VL53L0X_XSHUT_GPIO_Port, VL53L0X_XSHUT_Pin, GPIO_PIN_SET);
HAL_Delay(1000);
}
/**
* @brief Get distance from VL53L0X proximity sensor.
* @retval Distance in mm
*/
static uint16_t VL53L0X_PROXIMITY_GetDistance(void)
{
VL53L0X_RangingMeasurementData_t RangingMeasurementData;
// TODO - Error handling
VL53L0X_PerformSingleRangingMeasurement(&Vl53Instance, &RangingMeasurementData);
return RangingMeasurementData.RangeMilliMeter;
}Additionally attached the vl53l0x_tof.c file where the SetupSingleShot function is defined.
Basically it is all the same as in the nucleo example mentioned in the first post.
Regards, Lukas