cancel
Showing results for 
Search instead for 
Did you mean: 

Wiring a VL53L1X Breakout board, the datasheet (attached) confuses me

JamesTheEighth
Associate II

Hi,
I bought a VL53L1X Breakout board ToF sensor that I want to connect to a Raspberry Pi 3.
I need to connect the VIN, GND, SDA and SCL.
The documentation shows which pins are what, but it confuses me, as the layout in the documentation seems to be different than the boards itself.

Of the 10 pin holes on the board, one hole has a square around it, indiciating that would be pin 1. Across would be pin 2, and then on to the next row for the rest.
The square is on the outside column of the board.
However in the documentation pin 1 is on the inside column of the board.

What is the correct way to connect this?
VIN isn't specified on the board, does it have adifferent name?

I'm new to all of this, so I'm sorry if I ask the obvious.
Any help much appreciated.


1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

In Andrew Neil's reply remove the question marks. He's exactly right. 

There is a user manual:

How to use the VL53L1 with STMicroelectronics' X-CUBE-TOF1 Time-of-Flight sensor software packages for STM32CubeMX - User manual

that shows:

 

We built those satellite boards to fit directly onto the X-Nucleo boards.

the datasheet of the X-Nucleo board shows:

JohnEKVAM_0-1743433766434.png

And that should make it clearer. 

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

9 REPLIES 9
Andrew Neil
Super User

You mean this: https://www.st.com/en/evaluation-tools/vl53l1x-satel.html ?

 


@JamesTheEighth wrote:

Of the 10 pin holes on the board, one hole has a square around it, indiciating that would be pin 1. Across would be pin 2, and then on to the next row for the rest.

Indeed.

Also, looking at the board & carrying on with that counting would say that pin 6 must be ground:

AndrewNeil_3-1743429332837.png

Which corresponds to the Data Brief:

AndrewNeil_4-1743429422203.png

 

 


@JamesTheEighth wrote:

However in the documentation pin 1 is on the inside column of the board.


Which document are you referring to?

I only see that DB3555 Data Brief, and the only board layout in that is the photo:

AndrewNeil_1-1743429102611.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thank you for responding so swiftly.
I am indeed referencing the DB 3555 Rev2 manual, it has the diagram on page 3.

I read about the pin order and the little square on Chatgpt, so I want to double check:
Is the square indeed  on all PCB's always number 1, and is number two always next to it?

You said you could tell 6 is the ground by looking at the board. Is that because of the four tiny dots around it?

Thanks!







John E KVAM
ST Employee

In Andrew Neil's reply remove the question marks. He's exactly right. 

There is a user manual:

How to use the VL53L1 with STMicroelectronics' X-CUBE-TOF1 Time-of-Flight sensor software packages for STM32CubeMX - User manual

that shows:

 

We built those satellite boards to fit directly onto the X-Nucleo boards.

the datasheet of the X-Nucleo board shows:

JohnEKVAM_0-1743433766434.png

And that should make it clearer. 

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
JamesTheEighth
Associate II

I forgot to confirm, it's indeed about the part that you linked at the beginning of your message.


@JamesTheEighth wrote:

I am indeed referencing the DB 3555 Rev2 manual, it has the diagram on page 3.


you mean this:

AndrewNeil_0-1743435584467.png

That's a schematic - there's nothing on that which specifies physical positioning.

Schematics are about connections - not physical layout.

They are topological - not topographical.

 


@JamesTheEighth wrote:

Is the square indeed  on all PCB's always number 1


It is a common practice.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@John E KVAM wrote:

He's exactly right. 


Thanks!

ST are by no means the only ones guilty of this - this is an all too common documentation fail.

Pin numbering needs to be explicitly and clearly defined:

  • Where is pin one?
  • How does the numbering go from there?

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@JamesTheEighth wrote:

You said you could tell 6 is the ground by looking at the board. Is that because of the four tiny dots around it?


If you look closely, you can see that they're not just dots - they are connections to the ground plane:

AndrewNeil_1-1743436256815.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

okay that's very clear thank you

amazing, learned something new!