Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VD66GY with IMX8M Mini

Hello ST Brightsense Team,Would like to know if the VD66GY Linux driver (STSW-IMG503_V4L2) will work on an NXP IMX8M Mini (no hardware ISP) ?  If not will it work with the IMX8M Mini Plus (with Hardware ISP).Currently using the STEVAL-66GYMAI.In the ...

FB__1 by Associate III
  • 728 Views
  • 4 replies
  • 0 kudos

Resolved! vl53l8cx_def.h File

Hello,   I am having a hard time finding which software pack this file vl53l8cx_def.h is in? I think once I get that I should be get the zones if Im understanding the error correctly. Please advise.  If it helps with the solution I am trying to use t...

Rhagg28_0-1759612867921.png
Rhagg28 by Associate II
  • 882 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L8 firmware loading

I need to cut off all the power supplys of VL53L8 to save power. Does the firmware need to be re-downloaded every time the device is powered on? loading firmware is in the function uint8_t vl53lmz_init( VL53LMZ_Configuration *p_dev)​

Resolved! Does the noise affect measurements on VL53L0X?

Hi everyone,I'm working with the VL53L0X sensor and have a couple of questions:Does noise affect the sensor's measurements? Does the sensor include a checksum or mechanism to verify the integrity of I2C messages? Can adding capacitors to the I2C bus ...

Resolved! VL53L7CX blinded by retroreflective surface

I'm using several VL53L7CX sensors in a robotics application.  They work well except for when a retroreflective surface is present, which blinds the entire sensor, including SPADs not pointed at the retroreflective surface.  A large retroreflective a...

ayeiser by Associate II
  • 1550 Views
  • 5 replies
  • 5 kudos

Resolved! About IR smart upscale for VB1940 camera

Hi ST Support. The VB1940 camera has IR smart upscale.I think IR smart upscale separates only the IR data from RGBNIR and compensates for any missing data.Is there a way to send IR data without interpolating this missing data (without changing the im...

Resolved! P-NUCLEO-53L8A1 and VL53L8CHV0GC

I was looking to wire these 2 items together to acquire a LiDAR 3d point cloud data set for a research project im working. I wanted to get some input, feedback and guidance on utilizing this hardware for LiDAR 3d point clouds? VL53L8CHV0GCP-NUCLEO-53...

Rhagg28 by Associate II
  • 1071 Views
  • 5 replies
  • 3 kudos

BUG: VL53L1X API for uC where int is 16 bits (AVR)

Hi, I asked for help because my measurements took >> 15 seconds (up to 30s) in:https://community.st.com/t5/imaging-sensors/vl53l1-measurement-takes-up-to-30-seconds/td-p/843640Now after hours of debugging i found a bug in the API at least for platfor...