CLE.11
Associate
since
2021-08-02
2023-06-14
User statistics
1
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About CLE.11
Options
Report User
User Activity
Posts
Replies
I am trying to wire the VL53L1X-SATEL breakout board to a microcontroller (ESP32) yet the pinout is not clearly defined (even in the datasheet). Is VDD supposed to be the voltage input (between 2.8V and 5V) ?
2021-08-02
If the VDD pin on the left (breakable) part of the breakout board actually is the input voltage, then there is a problem, for the voltage drops and it even causes a brownout.
No replies to display.