Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X returns 0x1FFFF (8191)

Hello, I'm using a VL53L0X and it returns 0x1FFFF depending on whether a function within "VL53L0X_StaticInit" is commented or not during initialization. If "VL53L0X_set_reference_spads" is commented, the sensor sends values (with a large offset). But...

0690X00000D96y2QAB.png

Resolved! VL53L5CX LPn pin behavior/usage

I'm testing the VL53L5CX and finding that the behavior of the LPn pin differs from what is described in the datasheet. The datasheet says "Drive this pin to logic 0 to disable the I2C comms when the device is in LP mode. Drive this pin to logic 1 to ...

kwc by Associate III
  • 2097 Views
  • 1 replies
  • 0 kudos

Lowering power consumption

Hi,I am currently implementing an application using VL53L1X sensor with NRF52. Our applicaiton needs to consume very low current in order to get long battery life. I am reading VL53L1X sensor data every minute. While i am not reading any VL53L1X data...

TGund by Associate
  • 2353 Views
  • 4 replies
  • 0 kudos

Estmated max size of parameters

I'm referencing to STSW-IMG009 and specifically function VL53L1X_SetInterMeasurementInMs(uint32_t InterMeasMs)What would be the maximum size of the argument and the value of ClockPLL. I'm re-writing for another platform.Regards/Claes

Ckjel.1 by Associate
  • 997 Views
  • 1 replies
  • 0 kudos

[Proximity Sensor ADC with DMA Problem] I have GP2Y0A41SK0F Sharp for distance measuring sensor. the datasheet says it needs 16.5 ms with 3.7 ms tolerant. for sampling time. So I assumed I need to configure PCLK2 (I use ADC2), ADC Clock Prescaller, ...

channel sampling, then calculate those parameters until 16.5 ms found. The problem is kinda impossible to get 16.5 ms even I tried to adjust those parameter. anyone has a clue? Iam using STM32F407VGx