cancel
Showing results for 
Search instead for 
Did you mean: 

Teseo-VIC3DA dead reckoning mode

Fan1
Associate III

Hi,

I bought a Teseo-VIC3DA Evaluation Kit and when I went through the associated documents, they mentioned the concepts of "Teseo-DRAW and Teseo-DRUM". In my application, we do not have access to the vehicle's wheelticks/direction information so I guess I need to use DRUM. But I could not find any information about how to configure the evaluation kit to work in DRUM. Are DRAW and DRUM two different firmware or two different modes?

Another question is about the DR calibration. I first updated the firmware to BINIMG_4.6.18.11_VIC3DA_ARM and did not change any configuration. Then I installed the kit to a vehicle and after half an hour driving, I could see $PSTMDR2 showed "system ready" and $GPGGA showed the DR was working with location readings (strangely $PSTMDRCAL did not show up anymore but that may be a separate topic). Then I pulled the kit off from the vehicle and put it in my office, and found that $PSTMDR2 still showed "system ready" and $GPGGA still showed the DR was working after a long time. My question is, if I installed the kit to another vehicle, do I need to first erase the previous calibration or the calibration will heal itself in the new vehicle?   

Thanks,

1 ACCEPTED SOLUTION

Accepted Solutions
Francesco Virlinzi
ST Employee

Hi

Are DRAW and DRUM two different firmware or two different modes?

The VIC3DA autonomously switches on DRUM more when no ODO information is provided.

From Host point of view no actions is required (neither configuration change is needed)

 

My question is, if I installed the kit to another vehicle, do I need to first erase the previous calibration or the calibration will heal itself in the new vehicle? 

 

Take care that when used on car the VIC3DA has to be strongly fixed to the car/platform. No relative movement/vibration there must be between the module and the car.

Moreover Calibration in background is an always-running task, therefore no erase is needed if you change installation/car... the module detects the new installation and will recalibrate its-self

 

Regards

 Francesco

View solution in original post

18 REPLIES 18
Francesco Virlinzi
ST Employee

Hi

Are DRAW and DRUM two different firmware or two different modes?

The VIC3DA autonomously switches on DRUM more when no ODO information is provided.

From Host point of view no actions is required (neither configuration change is needed)

 

My question is, if I installed the kit to another vehicle, do I need to first erase the previous calibration or the calibration will heal itself in the new vehicle? 

 

Take care that when used on car the VIC3DA has to be strongly fixed to the car/platform. No relative movement/vibration there must be between the module and the car.

Moreover Calibration in background is an always-running task, therefore no erase is needed if you change installation/car... the module detects the new installation and will recalibrate its-self

 

Regards

 Francesco

Fan1
Associate III

Thanks for the prompt response, Francesco.

Another minor problem is that, I tried to reduce the amount of the NMEA messages by sending two commands: "$PSTMSETPAR,1201,1,0*34" and "$PSTMSETPAR,1228,0,0*3E" which should only allow GPGNS message. Below is the response. You can see that both commands have OK response. However, many NMEA messages still remain. Again the firmware is the latest "BINIMG_4.6.18.11_VIC3DA_ARM".


$PSTMSETPAROK,1201*31
$PSTMSETPAR,1201,1,0*34
$PSTMSETPAROK,1228*3A
$PSTMSETPAR,1228,0,0*3E
$GNGNS,180940.000,4328.97990,N,08032.06154,W,ENEEN,00,99.0,0295.3,0.0,,*0A
$GPGST,180940.000,0.0,0.0,0.0,-0.0,0.0,0.0,0.0*4E
$GPGBS,180940.000,,,,,,,*5B
$GNGSA,A,1,,,,,,,,,,,,,99.0,99.0,99.0*1E
$GPRMC,180940.100,V,4328.97990,N,08032.06154,W,0.0,57.1,150124,,,E*56
$GPGGA,180940.100,4328.97990,N,08032.06154,W,6,00,99.0,295.34,M,0.0,M,,*79
$GPVTG,57.1,T,,M,0.0,N,0.0,K,E*3A
$PSTMPRES,0.0,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,*0C
$PSTMVRES,0.0,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,*0A

Francesco Virlinzi
ST Employee

Hi

Take care VIC3Da uses 3 message-list:

  • message-list-0 (CDB 201-228) for GNSS message
  • message-list-1 (CDB 210-229) for DR message
  • message-list-2 (CDB 211-230) for GPGGA and GPRMC message

Based on these message-list you can disable all the message.

If you don't see any change more probably you are disabling a message on the wrong message-list

Regards

 Francesco

Fan1
Associate III

I have set all these CDBs (228, 210, 229, 211, 230) to 0 and set CDB 201 to 1 (i.e. only allow GPGNS) but it does not have any effect. See the NMEA messages below.

And in the software instruction document 9https://www.st.com/resource/en/user_manual/um2791-teseovic3-software-instructions-stmicroelectronics.pdf), only message-list-0 has a field table in Table 219.  And message-list-1 and message-list-2 do not have the field tables.

 

$PSTMSETPAROK,1201*31
$PSTMSETPAR,1201,1,0*34
$PSTMSETPAROK,1228*3A
$PSTMSETPAR,1228,0,0*3E
$PSTMSETPAROK,1211*30
$PSTMSETPAR,1211,0,0*34
$PSTMSETPAR,1190,0x01*5B
$PSTMGETPAR,1190*2A
$PSTMSETPAR,1201,0x00000001*50
$PSTMGETPAR,1201*21
$PSTMSETPAR,1228,0x00000000*5A
$PSTMGETPAR,1228*2A
$PSTMSETPAR,1191,0x01*5A
$PSTMGETPAR,1191*2B
$PSTMSETPAR,1210,0x00000000*51
$PSTMGETPAR,1210*21
$PSTMSETPAR,1229,0x00000000*5B
$PSTMGETPAR,1229*2B
$PSTMSETPAR,1192,0x01*59
$PSTMGETPAR,1192*28
$PSTMSETPAR,1211,0x00000000*50
$PSTMGETPAR,1211*20
$PSTMSETPAR,1230,0x00000000*53
$PSTMGETPAR,1230*23
$GPRMC,200530.400,V,4328.98696,N,08032.04397,W,0.0,61.2,170124,,,E*5E
$GPGGA,200530.400,4328.98696,N,08032.04397,W,6,01,99.0,295.34,M,0.0,M,,*74
$GPVTG,61.2,T,,M,0.0,N,0.0,K,E*3C
$GPRMC,200530.500,V,4328.98696,N,08032.04397,W,0.0,61.2,170124,,,E*5F
$GPGGA,200530.500,4328.98696,N,08032.04397,W,6,01,99.0,295.34,M,0.0,M,,*75
$GPVTG,61.2,T,,M,0.0,N,0.0,K,E*3C

Francesco Virlinzi
ST Employee

Hi

Are you working on UART or I2C?

I use the UART interface i.e. the micro-usb port on the Teseo-VIC3DA Evaluation Kit. I use the "$PSTMSETPAR" to set all the CDBs as in my last post and the module did return "$PSTMSETPAROK" message. Should it take effect immediately?

Hi

just a question: following all the $PSTMSETPAR commands you send.

Did you save on flash and reset? this is required to save the new configuration in flash and reset to load it during the boot and get it working.

you can do that with:

$PSTMSAVEPAR

$PSTMSRR

 

Ciao

 Francesco

Fan1
Associate III

I did not issue the commands "$PSTMSAVEPAR" and "$PSTMSRR" in my previous tests.

Now I sent these two commands after the $PSTMSETPAR commands. But the module stopped sending any message back after the reset (see below for the entire messages). Then I tried "$PSTMRESTOREPAR" to restore the factory setting but the module still did not send any message. It seems the module has stuck in a bad state. I may have to re-flash the binary. Are you able to confirm that the Section 12.17 to 12.19 of (https://www.st.com/resource/en/user_manual/um2791-teseovic3-software-instructions-stmicroelectronics.pdf) are accurate? It seems it is not the same as what you mentioned in your post of 2024-01-17 01:50 AM.

 

COM connected.
sendMessage: $PSTMGETSWVER,6*13 // sendMessage is the helper text from my program
sendMessage: $PSTMSETPAR,1201,1,0*34
sendMessage: $PSTMSETPAR,1228,0,0*3E
sendMessage: $PSTMSETPAR,1210,0,0*35
sendMessage: $PSTMSETPAR,1229,0,0*3F
sendMessage: $PSTMSETPAR,1211,0,0*34
sendMessage: $PSTMSETPAR,1230,0,0*37

$GPRMC,202605.000,A,4327.23196,N,08025.07693,W,0.0,358.2,190124,,,A*75
$GPGGA,202605.000,4327.23196,N,08025.07693,W,1,23,0.6,328.50,M,-34.9,M,,*5C
$GPVTG,358.2,T,,M,0.0,N,0.0,K,A*01
$PSTMVER,BINIMG_4.6.18.11_VIC3DA_ARM*3F
$PSTMGETSWVER,6*13
$PSTMSETPAROK,1201*31
$PSTMSETPAR,1201,1,0*34
$PSTMSETPAROK,1228*3A
$PSTMSETPAR,1228,0,0*3E
$PSTMSETPAROK,1210*31
$PSTMSETPAR,1210,0,0*35
$PSTMSETPAROK,1229*3B
$PSTMSETPAR,1229,0,0*3F
$PSTMSETPAROK,1211*30
$PSTMSETPAR,1211,0,0*34
$PSTMSETPAROK,1230*33
$PSTMSETPAR,1230,0,0*37

sendMessage: $PSTMSAVEPAR*58

$GPRMC,202605.100,A,4327.23196,N,08025.07693,W,0.0,358.2,190124,,,A*74
$GPGGA,202605.100,4327.23196,N,08025.07693,W,1,23,0.6,328.50,M,-34.9,M,,*5D
$GPVTG,358.2,T,,M,0.0,N,0.0,K,A*01
$GPRMC,202605.200,A,4327.23196,N,08025.07693,W,0.0,358.2,190124,,,A*77
$GPGGA,202605.200,4327.23196,N,08025.07693,W,1,23,0.6,328.50,M,-34.9,M,,*5E
$GPVTG,358.2,T,,M,0.0,N,0.0,K,A*01
$GPGGA,202605.000,4327.23196,N,08025.07693,W,1,23,0.6,328.50,M,-34.9,M,,*5C
$GNGNS,202605.000,4327.23196,N,08025.07693,W,ANAAN,23,0.6,0328.5,-34.9,,*29
$GPRMC,202605.300,A,4327.23196,N,08025.07693,W,0.0,358.2,190124,,,A*76
$GPGGA,202605.300,4327.23196,N,08025.07693,W,1,23,0.6,328.50,M,-34.9,M,,*5F
$GPVTG,358.2,T,,M,0.0,N,0.0,K,A*01
$GPRMC,202605.400,A,4327.23196,N,08025.07693,W,0.0,358.2,190124,,,A*71
$GPGGA,202605.400,4327.23196,N,08025.07693,W,1,23,0.6,328.50,M,-34.9,M,,*58
$GPVTG,358.2,T,,M,0.0,N,0.0,K,A*01
$PSTMSAVEPAROK*5C
$PSTMSAVEPAR*58
sendMessage: $PSTMSRR*49

COM disconnected.

Hi

I just tested the following scripts:

 

$PSTMCFGMSGL,0,1,1,0
$PSTMCFGMSGL,1,1,0,0
$PSTMCFGMSGL,2,1,2,0

$PSTMSAVEPAR

$PSTMSRR

 

Which sets:

 > $PSTMCFGMSGL,0,1,1,0 => GPGNS on message-list-0

> $PSTMCFGMSGL,1,1,0,0 => No DR message 

> $PSTMCFGMSGL,2,1,2,0 => GPGGA on message-list-2

 

and it works fine on my side.

Hope this helps

Regards

 Francesco