cancel
Showing results for 
Search instead for 
Did you mean: 

SPC56EL54 - RESET pin is always  pulled down by the CPU

GabiPaz-GSP
Associate II
Hi
On power up the SPC56EL54L5CBFS looks like it is in an internal RESET mode that does not  end. 
The RESET pin is always  pulled down by the CPU. 
Power up of 1.2v and 3.3v in 1.5msec.
 
Can you help to to understand why the RESET pin is always  pulled down by the CPU?
 
Thank you.
5 REPLIES 5
Peter BENSCH
ST Employee

Welcome @GabiPaz-GSP, to the community!

The RESET pin has an internal pull-down. What have you connected externally to the RESET pin?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter

Thank you, hope that you can help.

1K as pull-up and 10nF  to GND.

The 1.2v and 3.3v provided with 2 DC/DC converters.

 

Peter BENSCH
ST Employee

OK, at least externally RESET is obviously wired correctly.

However, RESET is a bidirectional pin whose internal open drain can be activated by various internal sources. As no information on software etc. is currently available, nobody can make a statement.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter 

After some testing,

 Internal RESET released after  Power up sequence.   
The Power up sequence should be as following:  3.3V , 1.2v PLL , delay : +500uS - 1.2v Core 
Can you please advice if this  Power up sequence OK?
Gabi

As far as I know, the order does not play a role during power up, you can also switch them on simultaneously.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.