"TeseoSuitePro_6_1_3" suite firmware bin correct? STA8090_v4.5.12.1_D1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 1:59 AM
I have the "TeseoSuitePro_6_1_3" suite. It comes with installed bin files for STA8089GAT. After I flash the firmware that arrives with the tool I get the tool to start , it sees the GPS satellites with good levels but it never gets a fix. I am also able to configure it to see Galileo but still no fix. What is wrong? is it a bad firmware? The suite reports: STA8090_v4.5.12.1_D1
Also mentioning our flash device is a 128M part MX25U12835FBBI-10G
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 5:04 AM
In Teseo-Suite:
Menu-Tools -> FW Configuration -> Read bin image configuration
It will open a panel where you can to provide the original firmware and from that it will generate a txt file with the whole configuration (save the file like cfg.txt)
The text file is
100 -> 00
101 -> 02
...
it means CDB-100 equals 00... CDB-101 eqral 02 etc...
in the cfg.txt file change the line (CDB) 249:
it is like:
249 -> 00000001
it has to be changed in
249 -> 00000000
save the file like new_cfg.txt
Now again in the Teseo-Suite:
Menu-Tools -> FW Configuration -> Writebin image configuration
in this panel providing:
- a binary firmware
- a text configuration file (the new_cfg.txt jsut saved)
it generates a new firmware which embeds the new configuration.
reflash the new binary in the device.
Take care that I'm suggesting the CDB-249 (not 250) to totally disable the flash protection.
Let me know
CIao
Francesco
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 2:44 AM
Hi
It seems to me the system is not saving the ephemeris data in the flash, due to that with empty ephemeris you'l never get a fix (also if you see good signal levels)
Which SPI flash are you using?
Thansk
Regards
Francesco
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 2:50 AM
We are aware that the flash we are using is not in the recommended devices list.
Our flash device is a 128M part MX25U12835FBBI-10G
Is these a way to verify or change a configuration to enable it to work?
It is strange as we are fashing the firmware on it and it is loading.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 3:04 AM
Hi
During the booting from SPI/SQI the application enables also the flash protection to avoid corruption of the binary code.
Just for test could you try setting CDB-250 = 0x8000000A (do that in the original binary and reflash from zero)
It's the value required for MX25U1635E / MX25U1635F.
Let see if it works also for MX25U12835FBBI-10G
Hope this helps
Regards
Francesco
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 3:09 AM
Hi Francesco,
Sorry for being a newbie here.
Could you please guide me how exactly do I set it in the original binary?
Thank YOU!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 3:16 AM
The SPM table for the 128M flash we use looks different than the 32M device.
See below table from 128M flash device:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 5:04 AM
In Teseo-Suite:
Menu-Tools -> FW Configuration -> Read bin image configuration
It will open a panel where you can to provide the original firmware and from that it will generate a txt file with the whole configuration (save the file like cfg.txt)
The text file is
100 -> 00
101 -> 02
...
it means CDB-100 equals 00... CDB-101 eqral 02 etc...
in the cfg.txt file change the line (CDB) 249:
it is like:
249 -> 00000001
it has to be changed in
249 -> 00000000
save the file like new_cfg.txt
Now again in the Teseo-Suite:
Menu-Tools -> FW Configuration -> Writebin image configuration
in this panel providing:
- a binary firmware
- a text configuration file (the new_cfg.txt jsut saved)
it generates a new firmware which embeds the new configuration.
reflash the new binary in the device.
Take care that I'm suggesting the CDB-249 (not 250) to totally disable the flash protection.
Let me know
CIao
Francesco
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 5:17 AM
Hi,
You advise gave us the clues we needed.
I actually changed only CDB-250 to 00000015 and now we have a fix. CDB-249 has the default value (enabled).
Is that a good setting?
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 5:25 AM
Hi
This confirm the issue was related to the flash-protection.
> CDB-250 to 00000015
To be honest I was thinking to 0xA because the values for MX25U1635E/MX25U1635F
Why are you using 0x15?
> Is that a good setting?
I don't know. You are using an un-tested SQI-flash.
Personally I would suggest... keep it running for a long time.... and try also standby operations.
Just a question: why are you using an unsupported memory?
Thanks
Regards
Francesco
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 5:46 AM
In the document "SQI flash protection application note" it is shown further down the table that Macronix MX25L3233F and similar parts, also with the T/B field, use the 0x15 value. The MSB bit has to be '0' otherwise the lower byte value is ignored (a NOTE in the firmware guide: "when enabled the value configured in B0..B30 is not used").
This was an initial design that used 1.8V i/o and the 128M flash part was readily available.
We will not use this flash in future designs.