cancel
Showing results for 
Search instead for 
Did you mean: 

"TeseoSuitePro_6_1_3" suite firmware bin correct? STA8090_v4.5.12.1_D1

Dror
Associate III

I have the "TeseoSuitePro_6_1_3" suite. It comes with installed bin files for STA8089GAT. After I flash the firmware that arrives with the tool I get the tool to start , it sees the GPS satellites with good levels but it never gets a fix. I am also able to configure it to see Galileo but still no fix. What is wrong? is it a bad firmware? The suite reports: STA8090_v4.5.12.1_D1

Also mentioning our flash device is a 128M part MX25U12835FBBI-10G

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

In Teseo-Suite:

Menu-Tools -> FW Configuration -> Read bin image configuration

It will open a panel where you can to provide the original firmware and from that it will generate a txt file with the whole configuration (save the file like cfg.txt)

The text file is

100 -> 00

101 -> 02

...

it means CDB-100 equals 00... CDB-101 eqral 02 etc...

in the cfg.txt file change the line (CDB) 249:

it is like:

249 -> 00000001

it has to be changed in

249 -> 00000000

save the file like new_cfg.txt

Now again in the Teseo-Suite:

Menu-Tools -> FW Configuration -> Writebin image configuration

in this panel providing:

  • a binary firmware
  • a text configuration file (the new_cfg.txt jsut saved)

it generates a new firmware which embeds the new configuration.

reflash the new binary in the device.

Take care that I'm suggesting the CDB-249 (not 250) to totally disable the flash protection.

Let me know

CIao

Francesco

View solution in original post

9 REPLIES 9
Francesco Virlinzi
ST Employee

Hi

It seems to me the system is not saving the ephemeris data in the flash, due to that with empty ephemeris you'l never get a fix (also if you see good signal levels)

Which SPI flash are you using?

Thansk

Regards

Francesco

Dror
Associate III

We are aware that the flash we are using is not in the recommended devices list.

Our flash device is a 128M part MX25U12835FBBI-10G

Is these a way to verify or change a configuration to enable it to work?

It is strange as we are fashing the firmware on it and it is loading.

Francesco Virlinzi
ST Employee

Hi

During the booting from SPI/SQI the application enables also the flash protection to avoid corruption of the binary code.

Just for test could you try setting CDB-250 = 0x8000000A (do that in the original binary and reflash from zero)

It's the value required for MX25U1635E / MX25U1635F.

Let see if it works also for MX25U12835FBBI-10G

Hope this helps

Regards

Francesco

Dror
Associate III

Hi Francesco,

Sorry for being a newbie here.

Could you please guide me how exactly do I set it in the original binary?

Thank YOU!

Dror
Associate III

The SPM table for the 128M flash we use looks different than the 32M device.

See below table from 128M flash device:

0690X000009XdZHQA0.png

In Teseo-Suite:

Menu-Tools -> FW Configuration -> Read bin image configuration

It will open a panel where you can to provide the original firmware and from that it will generate a txt file with the whole configuration (save the file like cfg.txt)

The text file is

100 -> 00

101 -> 02

...

it means CDB-100 equals 00... CDB-101 eqral 02 etc...

in the cfg.txt file change the line (CDB) 249:

it is like:

249 -> 00000001

it has to be changed in

249 -> 00000000

save the file like new_cfg.txt

Now again in the Teseo-Suite:

Menu-Tools -> FW Configuration -> Writebin image configuration

in this panel providing:

  • a binary firmware
  • a text configuration file (the new_cfg.txt jsut saved)

it generates a new firmware which embeds the new configuration.

reflash the new binary in the device.

Take care that I'm suggesting the CDB-249 (not 250) to totally disable the flash protection.

Let me know

CIao

Francesco

Hi,

You advise gave us the clues we needed.

I actually changed only CDB-250 to 00000015 and now we have a fix. CDB-249 has the default value (enabled).

Is that a good setting?

Thank you.

Hi

This confirm the issue was related to the flash-protection.

> CDB-250 to 00000015

To be honest I was thinking to 0xA because the values for MX25U1635E/MX25U1635F

Why are you using 0x15?

> Is that a good setting?

I don't know. You are using an un-tested SQI-flash.

Personally I would suggest... keep it running for a long time.... and try also standby operations.

Just a question: why are you using an unsupported memory?

Thanks

Regards

Francesco

In the document "SQI flash protection application note" it is shown further down the table that Macronix MX25L3233F and similar parts, also with the T/B field, use the 0x15 value. The MSB bit has to be '0' otherwise the lower byte value is ignored (a NOTE in the firmware guide: "when enabled the value configured in B0..B30 is not used").

This was an initial design that used 1.8V i/o and the 128M flash part was readily available.

We will not use this flash in future designs.