| Subject | Author | Posted | |
|---|---|---|---|
|
We're trying to get a 3 phase, 18 pole pair, <150V <5A motor going. When we try to start with evspi...
| 2024-12-04 1:48 AM | ||
|
Hello, I am currently working with the STM Motor Control SDK (version 5.4.8) and noticed that it o...
| 2024-12-03 1:47 AM | ||
|
For steval esc001v1 with MC workbench Version: 6.3.0, to run firmware do we need any other connecti...
| 2024-12-03 1:01 AM | ||
|
I'm trying to use a RS422 transceiver set up between ST Motor Pilot and EVSPIN32G4 development boar...
| 2024-12-02 8:43 AM | ||
|
Hello, I want to control the evaluation board using the serial protocol? Where is the documentati...
| 2024-12-02 7:33 AM | ||
|
When I parse the data sent according to the motor protocol, I find that it is completely different ...
| 2024-11-28 5:37 PM | ||
|
I am having false Over Current conditions when the inverter board starts up, before any kind of ope...
| 2024-11-28 8:13 AM | ||
|
I am newbie of mc workbench. I'm in trouble with making custom board configuration of MC workbench...
| 2024-11-28 2:56 AM | ||
|
Hello I need help for STSPIN32G4 EMI Issue I took tests for Farfield EMI Report at STSPIN32G4 Stan...
| 2024-11-27 11:58 PM | ||
|
Is there any support for evspin958 connected to the Nucleo-G071 board? I’m not really sure how to p...
| 2024-11-27 7:27 AM | ||
|
MCSDK v6.3.2 It looks like the STM32 is failing to PWM fet gates and that's resulting in high c...
| 2024-11-21 2:04 PM | ||
|
Hello everyone, I am utilizing the IHM08M1 board for a Voltage Source Converter (VSC) academic p...
| 2024-11-14 5:47 AM | ||
|
[VERSION]: MCSDK 6.3.1 & 6.3.2 [TOOL]: MCWB, Motor Pilot Zip file contains MCWB project file and ...
| 2024-11-11 10:43 AM | ||
|
Hello I am currently doing a project that require to control a BLDC motor with an STM32 MCU car...
| 2024-11-08 12:43 AM | ||
|
Hi all, We plan to implement STSPIN32G4 to our custom motor controller solution. For that purpose,...
| 2024-11-04 4:16 PM | ||
|
Hello ST Community, I'm using an X-NUCLEO-IHM17M1 shield with a NUCLEO-F401RE board to control a 6...
| 2024-10-25 10:28 PM | ||
|
Hello. I am running an x-nucleo-IHM03A1 with a Nucleo-F401RE and a 24BK20-30 Stepper motor. I hav...
| 2024-10-25 11:58 AM | ||
|
Hello, I am using the MC Workbench V6.3.1. When I generate the code and the profiler is activated,...
| 2024-10-22 9:36 AM | ||
|
I am using MC Workbench V6.3.1. The a few times after installing the software, I could generate the...
| 2024-10-22 7:05 AM | ||
|
A nice function would be if in the tab "Sensorless start-up parameters" new choice was added to us...
| 2024-10-16 4:52 AM |