cancel
Showing results for 
Search instead for 
Did you mean: 

Configurable open-loop instead of startup profile

Ricman666
Visitor

A nice function would be
if in the tab "Sensorless start-up parameters" new choice was added to use open-loop control insteand of startup profile where you could configure how much current/voltage at given speed in several steps and threshold to switch to closed-loop control.
It would be good if I want the motor to operate permanently at very low speeds and have the possibility to regulate the speed (same as open-loop control in motor pilot),
until the engine reaches the given speed(configurable treshold) it will automaticaly switch to closed loop control(6-step or FOC) in sensorless mode of course.

 

0 REPLIES 0