cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Pilot and FTDI RS422/485 - Is it possible?

Frakk2136
Associate III

I'm trying to use a RS422 transceiver set up between ST Motor Pilot and EVSPIN32G4 development board.
I'm using an FTDI USB-Serial converter and two RS422 Transceivers with /RE and DE signals.

Is it possible using the ST Motor Pilot to use these hardware flow control signals to set the transceivers in RX/TX modes as transmission occurs?

0 REPLIES 0