| Subject | Author | Posted | |
|---|---|---|---|
|
EDIT: Resolved! It looks like this was an issue with the pin reporting on our end. Hello, ...
| 2026-05-04 11:41 AM | ||
|
I recently built a motion-control setup using an STM32 MCU to drive a NEMA 23 stepper via a DM5...
| 2026-03-31 8:53 PM | ||
|
Are there any plans to make a Linux version of the Motor Control Workbench? @cedric H mentioned 4...
| 2026-02-19 2:53 AM | ||
|
Hi, I am working in steval-esc001v1. I have set the a2212-13t-1000kv bldc motor to ran at minimum ...
| 2026-02-16 9:42 PM | ||
|
Hi, How can one calculate the maximum phase current of a BLDC motor using sinusoidal control with ...
| 2026-01-23 12:36 AM | ||
|
Hello everyone,
I am using the STMicroelectronics IHM16M1 motor driver board with STM32 MC Workbe...
| 2025-12-28 6:54 PM | ||
|
Hi - I'm about to start in on a new motor control application using ST Micro products. Can anyone s...
| 2025-12-14 4:41 PM | ||
|
Hi everyone, I’m new to STM32 and working on a custom board using the STSPIN32G4 to drive a 3-phas...
| 2025-12-07 10:52 AM | ||
|
Hi, I am using encoder mode TI1 and TI2 on TIM1 and TM3 to read encoder, however the polarity is ju...
| 2025-11-19 7:55 PM | ||
|
Hello Expert,
I am reaching out regarding some persistent issues I am facing with MCSDK 6.41 on t...
| 2025-11-13 4:17 PM | ||
|
Hi everybody! I started programming ARM microcontrollers after watching Mr. Patrick Hood-Daniels' ...
| 2025-10-25 7:29 PM | ||
|
Hi ALL, I'm working on a MCSDK project which configures as follow: 1. STM32F407VET6 (yes I migrat...
| 2025-10-01 10:09 AM | ||
|
Issue 1: file: hall_speed_pos_fdbk_sixstep.c function: HALL_TIMx_CC_IRQHandler() line: 393 The ...
| 2025-09-18 1:15 AM | ||
|
Dear MCSDK users,
The full MCSDK documentation is embedded in the Motor Control Workbench too...
| 2025-07-29 8:15 AM | ||
|
Hello, I am using the FOC with hall sensor (having at 15 degree mechanical accuracy) on a BLDC m...
| 2025-06-12 1:57 AM | ||
|
I made customized board based on bg431besc1 board all pin defined are same as original board excep...
| 2025-05-29 12:35 AM | ||
|
Dear STM Community, I am currently developing an elevator door control application using the EVSPI...
| 2025-04-25 1:54 AM | ||
|
I have a custom design using SDK 6.3.2 that was started by modifying the board files from NUCLEO-L4...
| 2025-03-06 4:42 PM | ||
|
Hello community Please help me, i am facing issue related to injected ADC on PWM timer MCU : stm...
| 2025-03-06 2:49 AM | ||
|
Hello, We've designed a STSPIN32F0251-based motor driver board, but when running the 6-step firmwa...
| 2025-03-03 4:22 PM |