User Activity

I am working on a BLDC motor control project using ST MCSDK Workbench 5.4.7. The motor has 15 pole pairs.When I configure the system to use a quadrature encoder, I can rotate the motor and successfully control its speed in both directions using the W...
Hello,I am currently working with the STM Motor Control SDK (version 5.4.8) and noticed that it only supports STM32G474, while my project requires using the STM32G473 microcontroller.Is there an option to add STM32G473 as a new package to the SDK? If...