| Subject | Author | Posted | |
|---|---|---|---|
|
How to calculate the gain parameter of PI controller in PLL generated by workbench? After doing lot...
| 2024-07-10 11:53 PM | ||
|
Dear Team, I hope this message finds you well. I have succesfully control sensored hub motor in s...
| 2024-07-10 3:22 AM | ||
|
Hello, I am trying to implement a P-controller-algorithm for two levers, where one lever follows t...
| 2024-06-25 6:59 AM | ||
|
Hello! I am looking to run 4 industrial servo motors on any of the STM controllers (Any which can s...
| 2024-06-25 4:11 AM | ||
|
Hello. Trying to profile one of my engines with the ST Motor Pilot Tool (profiler) V1.2.9. Without ...
| 2024-06-24 2:59 AM | ||
|
After designing Motor controller, on what testcases we should test our Motor Controller? after g...
| 2024-06-22 2:28 AM | ||
|
I am testing the Standby mode with the EVSPIN32G4 board. However, it is not entering standby m...
| 2024-06-13 5:30 PM | ||
|
For our application, we are running the stepper motor from 5 step/sec to 6500 step/sec and to achie...
| 2024-06-11 10:27 PM | ||
|
My sensors polarity active low at my custom board I'm using a inverting schimitt trigger how can i ...
| 2024-06-07 8:54 AM | ||
|
Hello, I have a custom inverter board which is designed for high power applications 100A+. I have ...
| 2024-06-06 12:25 PM | ||
|
Hello, I have following problem: I generated a project using MC Workbench (6.3) and everything wor...
| 2024-05-31 8:45 AM | ||
|
Hi, if i want to use PWM out for my motor driver inverter complement of each other. Can i configu...
| 2024-05-16 10:54 PM | ||
|
What's the maximum/minimum electrical parameters for the motors that can be used with the MCSDK? E...
| 2024-05-16 7:50 AM | ||
|
Hello everyone, I ran into a problem when re-generating a project in a СubeMX. If I make some upda...
| 2024-05-14 3:35 AM | ||
|
Hi all! I'm currently developing my own motor control board and have encountered a problem with ru...
| 2024-05-11 9:50 AM | ||
|
Using a 2804 gimbal motor, and the specifications provided by the vendor are as follows. The p...
| 2024-05-10 7:44 PM | ||
|
I would like to implement a feature,During motor operation,Increasing loads,By controlling the rota...
| 2024-05-09 9:49 AM | ||
|
i use the p-nucleo-ihm006 board to run open-loop mode, it runs well in low speed; but when run in h...
| 2024-05-05 2:10 AM |