| Subject | Author | Posted | |
|---|---|---|---|
|
Hello STM Community, We are developing a custom motor driver board based on the STSPIN32F0251 and ...
| 2025-02-07 12:46 PM | ||
|
When I increase the speed of the stepper motor, it sometimes changes direction on its o...
| 2025-01-29 2:54 AM | ||
|
Hi, I am trying to run a 3-phase BLDC motor using the DRV8323 driver in 1xPWM mode with a Hall...
| 2025-01-17 1:01 AM | ||
|
I am trying to output a 3-phase PWM waveform with a phase difference of 120 degrees using one timer...
| 2025-01-15 8:27 PM | ||
|
Good morning.
I am running an IHM03A1 stacked onto a Nucleo - WB55RG. I am finding that if I sen...
| 2025-01-10 8:07 AM | ||
|
As my understanding, ST890 used for isolate USB 5V and Battery 5V( DC/DC from 10V by U12: LDFPVR )....
| 2025-01-10 6:03 AM | ||
|
Hi I have a question. I wanna get to multiple value using RCM Function. main.c I...
| 2025-01-07 5:30 PM | ||
|
Hi ST Team, Happy new year and I managed to connect and get the motor somewhat running! How...
| 2025-01-06 9:56 PM | ||
|
Board: Nucleo-STM32F401 + Nucleo-IMH021A Motor: PKP246D15A2-R2FL Firmware: X-CUBE-SPN2 V1.1.1 Po...
| 2025-01-05 4:59 PM | ||
|
Hello Community, I’m using NUCLEO F302R8 and IHM08M1 for motor control. While the motor runs, ...
| 2025-01-04 3:45 AM | ||
|
Good morning.
I have an X-NUCLEO-IHM03A1 stacked onto a NUCLEO-WB55RG. During a power down I imm...
| 2025-01-03 7:28 AM | ||
|
We are operating the motor with the Run command “Run(DIR, SPD)” to rotate it at a constant speed. H...
| 2024-12-30 6:06 PM | ||
|
Hello everyone, How can I set a speed limiter when I use the motor in Torque Mode(FOC)?. I am gett...
| 2024-12-28 12:04 PM | ||
|
Hello, I encountered some issues while using SPI to control L6482: 1. My read/write SPI logic seem...
| 2024-12-24 5:39 PM | ||
|
Hello, I use the EVSPIN32G4 to test some brushless motors. On ST motor workbench there is an op...
| 2024-12-18 9:48 AM | ||
|
I am trying to implement a Phase Locked Loop in a microcontroller STM32. I have a reference signal ...
| 2024-12-18 3:40 AM | ||
|
Hello, I've tried to post a question in the motor control forum section, but probably with this...
| 2024-12-06 7:12 AM | ||
|
Hi, I have been looking for a reference design using ST's product for driving a sensorless BLDC Mo...
| 2024-12-04 6:05 AM | ||
|
Hi All, I met some issues in ST Motor profile. It showed me waning as below when i click connect....
| 2024-12-04 6:00 AM | ||
|
Hello everyone, I would like to understand about MC library and some motor control terms. 1 - I ...
| 2024-12-04 4:46 AM |