Problem in single conversion mode in ADC
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-07-02 10:09 PM
Hi,
While implementing a single conversion process for the Analog-to-Digital Converter (ADC) via register-level programming, the debugging phase yields a consistent output of zero, irrespective of the input. This anomaly persists even after the ADC input pin PC0 is alternated between a ground (GND) connection and a 3.3V supply, indicating no variation in the output value.
I am using Nucleo-L476RG evaluation board.
Please help.
Here is my code:
#define ADCEN (1U << 13)
#define GPIOCEN (1U << 2)
#define ADC_CH1 (1U << 6)
#define ADC_SEQ_LEN_1 0x000
#define CR_ADEN (1U << 0)
#define CR_ADSTART (1U << 2)
#define ISR_EOC (1U << 2)
#define CR_ADCAL (1U << 31)
void pc0_adc1_init(){
RCC -> AHB2ENR |= GPIOCEN;
GPIOC -> MODER |= (1U << 0);
GPIOC -> MODER |= (1U << 1);
RCC -> AHB2ENR |= ADCEN;
ADC1 -> CR &= ~CR_ADEN;
ADC1 -> CR |= CR_ADCAL;
while(ADC1 -> CR & CR_ADCAL){}
ADC1 -> SQR1 |= ADC_CH1;
ADC1 -> SQR1 |= ADC_SEQ_LEN_1;
ADC1 ->CR |= CR_ADEN;
}
void adc_conversion(void){
ADC1 -> CFGR |= CFGR_CONT;
ADC1 -> CR |= CR_ADSTART;
}
uint32_t adc_read(void){
while(!(ADC1 -> ISR & ISR_EOC)){}
return (ADC1 -> DR);
}
uint32_t sensor_value;
int main(void){
pc0_adc1_init();
adc_conversion();
while(1){
sensor_value = adc_read();
}
}
View more
Labels:
- Labels:
-
ADC
-
STM32L4 series
0 REPLIES 0