| Subject | Author | Posted | |
|---|---|---|---|
|
The software drives the SPI to drive the RF chip, and I add a 0r resistor to the SPI as shown in Fi...
| 2024-06-19 5:10 AM | ||
|
Hello everyone, I have a stm32l072 microcontroller and an NB exs82 module connected via LPUART. And...
| 2024-06-19 4:53 AM | ||
|
Dear Community Support, Recently, our team acquired an STLINKV3 debugger (MB1440 + MB1441) with...
| 2024-06-17 8:58 PM | ||
|
Hi all, I'm working with STM32F4 disc board, I'm using PB8 and PB9 as interrupt input, those pin s...
| 2024-06-17 6:17 AM | ||
|
I recently started working on a custom board project based on an STM32G070CBT and using the SWD i...
| 2024-06-17 5:10 AM | ||
|
Hi, I try to configure a STM32C031K6 to generate an interupt every seconds using RTC Alarm A (RTC ...
| 2024-06-14 6:56 AM | ||
|
Hi, I have the STM32H753i-EVAL2 and need to boot from TFTP using U-BOOT. As the STM32H743i-EVAL is...
| 2024-06-13 8:53 AM | ||
|
Hi,
I am using Olimex STM32-E407 evaluation board which has STM32F407ZG. I tried Freertos,LWip et...
| 2024-06-13 4:55 AM | ||
|
i am using a stm32f401ccu6 board to receive modbus rtu requests from a master device(windows laptop...
| 2024-06-12 5:27 PM | ||
|
Hello, I want to use a OV7670 camera module with my STM32U585CIU6, which has no support for DCMI. ...
| 2024-06-12 5:45 AM | ||
|
When the bootloader is updated from the main appli, the start address at reset can be set to the st...
| 2024-06-11 11:31 PM | ||
|
Hi, I see an alias, using DFSDM (sinc3) and a PDM mic at 16kHz, while a speaker produces 1...24kHz...
| 2024-06-11 8:09 AM | ||
|
Hi, I'm attempting to use UART3 on a STM32L431CC to transmit 9 bit data, I've created the foll...
| 2024-06-11 1:51 AM | ||
|
Hello: This is weird problem. We have a STM32L496 system that handles multiple I2C devices through...
| 2024-06-10 12:47 PM | ||
|
Hi, We are using STM32L452CEU6 with 48QFPN package and trying implement sleep mode 2 inside Azure ...
| 2024-06-10 6:42 AM | ||
|
Please go and visit our wiki pages Basics of power supply design for MCU. This article covers gen...
| 2024-06-10 2:55 AM | ||
|
I am working on ble MS in B l4s5i iot kit. while searching the blog I got know how to connect it, a...
| 2024-06-10 12:35 AM | ||
|
Hi St-community
I'm having variations in temperature readings from the internal sensor on my STM3...
| 2024-06-10 12:34 AM | ||
|
Drivinng ann H bridge to generate a sinewave , PWM generated and driving the H bridge .The PWM siga...
| 2024-06-07 6:42 AM | ||
|
Hello, I have a relatively simple program where I am trying to go into stop 0 mode while my ADF us...
| 2024-06-06 6:29 PM |