Imaging (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Measuring Multiple vl53l4cd on single i2c line

I am currently implementing a series of  vl53l4cd sensors into a project. These work really well and I am able to address these individually on one shared i2c line. These sensors are working perfectly fine on this shared line when measured independen...

Varying data output of Vl53L1X

Hi,I am using Vl53L1x for a custom application. When i block the sensor with a black tape, i see that the data from getdistance or get signal rate function drops (increases for signal rate functn) after 1 min drastically. For example on blocking the ...

vishnusf by Associate II
  • 56 Views
  • 1 replies
  • 1 kudos

Ranging frequency of VL53L1X

HI,What is the definition of ranging frequency. Is it how fast it can make consecutive measurements?What is the highest ranging frequency (lowest inter measurement period) SPAD sensor that ur company provides?Thank u 

vishnusf by Associate II
  • 68 Views
  • 1 replies
  • 0 kudos

Signal Frequency of the SPAD sensor VL53L1X

Hi, I am using Getsignalrate function inorder to obtain the photon count of VL53L1X sensor. Could somebody tell me what the frequency of the actual signal is, ignoring the I2C and UART communication speed. Or the signal that we get is completely depe...

vishnusf by Associate II
  • 109 Views
  • 1 replies
  • 1 kudos

Documentation of X Cube Vl53l1A1

HI,I downloaded X cube 53l1A1 software. After extracting it i opened the documentation file I see that it is blank. Could u please provide assistance with this matter.Thank you

vishnusf by Associate II
  • 51 Views
  • 1 replies
  • 0 kudos

VL53L1X for custom use

HiI want to use VL53L1x board sensor for custom application. I wanted to use an external laser source of 940nm and block the onboard laser source. Are there any precautions to be taken for such case?I also wanted to know is it possible to access the ...

vishnusf by Associate II
  • 182 Views
  • 3 replies
  • 2 kudos

Resolved! VL53L7X get Point Cloud

Hi, I'm trying to create a 4x4 point cloud using a VL53L7CX-Sensor. I already got the x, y and z, but I am not sure if the values are right. My approach:*iter_x = static_cast<float>(kMillimeterToMeter * cos(w * fovPerPixel - kFov / 2.0f - DegToRad(90...

Hartm_Sve_0-1712560687133.png