Resolved! no spice model for opamp? TL062
Do ST has spice model for opamp ? Especially TL062
Do ST has spice model for opamp ? Especially TL062
please help to provide the SGS report of TSC200IST for Goertek
Hi,1. Is there a SPICE model available for this part?2. Is the output open-drain or push-pull? Cheers,Kay
Hello,We currently use diode 1N5711 in an array. It would be beneficial to have matched batches as mentioned on the website 1N5711 - 70 V, 15 mA RF and Ultrafast Switching Signal Schottky Diode - STMicroelectronics.I'd like to know more about the mat...
I have image of an IC and I am not able to identify what is the component and part number Please support.
Dear All,when we submit IMDS for SMA6T28CAY, we fail to mark polymeric parts as below. pls help to advise how we can make it. Thanks.IMDS #:190311
hello.I'm currently testing a 2-axis joystick connected to an ADC120.I want the X and Y axis values to go into IN0 and IN1, but only the X axis values go into all channels. The channel changes normally, but is it possible to separately input 2-ax...
Hi, I use ADC120 my new project, but device get only convert first channel. I change channel but its gives only first ch.There is a ST demo bord at web site but there is a no example code. How can i solve this problem.I read same topic in this web ...
Is L7805ABD2T-TR type A or B D2PAK? Ordering information doesnt have any designation to order Type A or B and I am not sure what type is L7805ABD2T-TR.
Hello together,We are using the TSV992A to measure a current across a 10mOhm shunt resistor. We use a non-inverting amplifier circuit with a gain of 17.6. With a voltage divider (10k-10k) we create an offset voltage at the In+ input.The amplifier is ...