2024-02-20 4:24 PM
Hi,
1. Is there a SPICE model available for this part?
2. Is the output open-drain or push-pull?
Cheers,
Kay
2024-02-23 7:07 AM
> 1. Is there a SPICE model available for this part?
It seems there's only the eDesignSuite link, I just tried it and that's quite useless, because TSV6392A can't be selected.
BUT the datasheet says something about a macro model...
> 2. Is the output open-drain or push-pull?
It's declared as an opamp, so that's usually push-pull.
2024-03-01 4:35 AM