Resolved! TSV912IQ2T absolute maximum input voltage
The following are some questions related to the absolute maximum ratings of the TSV912IQ2T which are not clear from the datasheet. Can the voltage on the input pins (2,3,5 and 6) swing to values greater than VCC + 0.2V (for example 50V) if the curren...