2024-05-01 05:25 AM - edited 2024-05-01 05:26 AM
What is the time zone of the forum. My last complaint is tagged "2024-05-01 5:21:40 AM" while here it is about 12:23:34 UTC 2024.
Please tag the posting explicit with the tinmezone!
2024-05-15 01:52 AM
Hi @Uwe Bonnes ,
Thanks for raising this question and apologies for a delayed response. The default time zone of the forum is: GMT -08.00 U.S. Pacific Time.
As @Tesla DeLorean correctly pointed out, the time zone can be adjusted based on your preferences via My settings > Preferences > Time zone. At this point of time, it is not possible to automatically adjust the time zone display, for example: based on your defined location on a profile.
I will check if there are any feature updates upcoming and get back.
2024-05-15 02:24 AM
Hello @Andrew Neil @Uwe Bonnes , @Tesla DeLorean ,
To cover the additional points in the discussion:
- The default time zone when logged out is the system one: GMT -08.00 U.S. Pacific Time.
- The one you set on your settings is only for the log-in view.
@Andrew Neil , thanks for pointing out the incorrect formatting, I will check if it is an easy fix and get back.
Greetings,
Lina
2024-05-15 03:17 AM
@Lina_DABASINSKAITE: So please tag the time with the correct timezone indicator!