2024-05-01 5:25 AM - edited 2024-05-01 5:26 AM
What is the time zone of the forum. My last complaint is tagged "2024-05-01 5:21:40 AM" while here it is about 12:23:34 UTC 2024.
Please tag the posting explicit with the tinmezone!
2024-05-15 1:52 AM
Hi @Uwe Bonnes ,
Thanks for raising this question and apologies for a delayed response. The default time zone of the forum is: GMT -08.00 U.S. Pacific Time.
As @Tesla DeLorean correctly pointed out, the time zone can be adjusted based on your preferences via My settings > Preferences > Time zone. At this point of time, it is not possible to automatically adjust the time zone display, for example: based on your defined location on a profile.
I will check if there are any feature updates upcoming and get back.
2024-05-15 2:24 AM
Hello @Andrew Neil @Uwe Bonnes , @Tesla DeLorean ,
To cover the additional points in the discussion:
- The default time zone when logged out is the system one: GMT -08.00 U.S. Pacific Time.
- The one you set on your settings is only for the log-in view.
@Andrew Neil , thanks for pointing out the incorrect formatting, I will check if it is an easy fix and get back.
Greetings,
Lina
2024-05-15 3:17 AM
@Lina_DABASINSKAITE: So please tag the time with the correct timezone indicator!
2024-10-25 10:33 AM
Any news on tagging all dates with the timezone?
2024-11-11 11:48 AM
Hi @Uwe Bonnes ,
Apologies for the silence on this one. Are you referring to the formatting issue brought by Andrew Neil? If yes, this issue has been addressed and we are waiting for the fix. Unfortunately, I can not give the exact date yet.
If this is about something else, let me know.
Best regards,
Lina
2024-11-12 2:18 AM
I will accept as solution when implemented...
2025-02-25 2:38 AM
Hi @Andrew Neil,
This is changed now. The "0" no longer appears by default.
Best regards,
Laurids
2025-02-25 3:48 AM
I do not see what has changed. I live in EST and it is around 13:45 now. On the community page a recent posting appeared as second entry from top with now view and answer:
So neither the TZ zone of the given time is given nor is the date translated into the users TZ
2025-02-25 3:57 AM
Otherwise if you perhaps mean that now "2025-02-25 3:42" is printed and befor perhasps "2025-02-25 03:42" I do not see any gain for users...
2025-02-25 4:43 AM
Hi @Uwe Bonnes,
Please check if the time zone setting is adjusted to fit your location in the preferences page.
Thanks,
Laurids