2023-11-09 6:40 PM - edited 2023-11-09 6:43 PM
Dragged a mouse accidentally over this post down there. Pressed at least one or both of the left/right mouse buttons at the same time. The screenshot has not been modified...
The only interaction with the page, that still works:
Happened on a Vivaldi browser, which is Chromium/Blink based.
2023-11-13 8:52 AM
Hello @Piranha ,
Thanks for reporting. I will pass it over to troubleshoot.
Regards,
Lina
2023-11-17 11:32 AM
Just happened to me, too. I'm not sure what caused it - I've scrolled down to the last post of the thread and then clicked a couple of times on it without thinking too much what am I doing, and boom, the whole thread went grey.
Win/FF
JW
2023-11-20 6:40 PM
And another slightly different one happened while editing a reply:
Pay attention to the "drop files" sections.
2023-12-06 5:32 AM
Hello, @Piranha , @waclawek.jan ,
Getting with some feedback here. We were not able to replicate this issue, so the recommendation would be to clearing the cache and cookies from the browser and see if the problem persists. If so, will ask you to screen record this behavior.
Thanks a lot,
Lina